Part Number: SN6507 Other Parts Discussed in Thread: SN6501 , SN6505B Tool/software: Hi TI Team
I have the design kit SN6507 from Wuerth-Elektronik and I tested it with my own requirements. I need an isolated psu for an 4-20mA loop.
Input voltage…
Part Number: SN6501-Q1 Other Parts Discussed in Thread: SN6501 , SN6505A Tool/software: Hi team,
Could you pls send me the EMI test report of SN6501-Q1? Thanks!
Best regards!
Ethan
Part Number: SN6501 Other Parts Discussed in Thread: SN6507 Tool/software: Hi experts,
Good day.
My customer wants to do 12V->12V, <1W power. They used SN6501 in old project before, and can it achieve 12V->12V? The input range is up to 5V from datasheet…
Part Number: SN6501 Other Parts Discussed in Thread: SN6507 Tool/software: Hi TI,
I am using the SN6501 IC. The following are the testing waveforms of VSW1, VSW2, and ISW1/2 under no load condition and approximately 4Vin. The testing currents should…
Part Number: SN6501-Q1 Other Parts Discussed in Thread: SN6501 , Hello Team,
is there any reason why the output voltage is limited to 30V according datasheet?
Depending on transformer ratio it should be possible to achieve higher voltages, right…
Part Number: SN6501 Other Parts Discussed in Thread: ISO6742 Hi team,
Could you please review this part on the schematic? It is on page 4, U3.
One thing that looks strange to me is I believe this can only provide a 3.3V or 5V isolated rail. However…
Part Number: SN6501 Hi Team
Could you please tell me the Vout accuracy of SN6501DBVR?
I'd like to judge if we need LDO or not.
The condition is below.
Turns Ratio = 1:1.1, Vin=5V, Vout=5V, No LDO