Part Number: SN6505A Hi team,
Can I know the internal pull-down resistance of EN pin? My customer wants to pull-up the EN pin and wants to know what's the best pull-up resistance.
Regards,
Xiaoying
Part Number: SN6505A Other Parts Discussed in Thread: SN6507 Hi Team:
My customer want to use SN6505A to make a 6W power module as 5V/1.2A.
But i check the spec of ILIM is more than 1.2A. so would you help to check whether we can reach to 1.2A ? and…
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6501 We are using SN6505 transformer driver in our project.
Original part was SN6501 and is being changed to SN6505 for better EMC performance.
We have question about how to terminate EN,…
Part Number: SN6505A-Q1 Tool/software: Hi experts,
When I tested the waveform of D1 pin and D2 Pin, Which is shown as below. Why the amplitude of them are 10V, I'm curious about the reason.
Best regards!
Ethan Liu
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: SN6505A , SN6505B , ISOUSB211 Hi Simulation team,
My customer has a problem SN6505A at PSpice. (As the responses in this link shows, an error occurs when trying to use the SN6505A model. https…
Part Number: SN6505A-Q1 For the figures entitled "Efficiency vs Load Current" (for example Figure 6-2), does the efficiency estimate include the losses from the diode?
Part Number: SN6505A Other Parts Discussed in Thread: UCC25800 , UCC25800-Q1 , SN6507 Hi, we are using the Würth 750315240 transformers in series to build a high voltage isolator.
It works really well with the LT3439, but now we want to try the 6505A…
Part Number: SN6505A Other Parts Discussed in Thread: SN6505B Hello
We inquire about the application of the SN6505A for below design.
1.Is it available to connect two transformers in parallel? if available, could you review the design?
2.Is it…
Part Number: SN6505A-Q1 Hi,
I am using the SN6505AQDBVTQ1 for an automotive DCDC but it is impossible to get any sample.
Have you got a solution?
Best regards
Yoann
Part Number: SN6505A-Q1 Other Parts Discussed in Thread: SN6505A , SN6505B Hello,
I am having an issue with my design, as shown below. The voltage at Pin.2 of the transformer (750313769) is pulling P5V0 from 5V to less than 2V and back to 2V to 5V.…