Hello Benjamin,
After reviewing your posts, I believe that you are on the right track and the thermal protection is most likely triggering and stopping the switching. Once the device cools down it tries to switch again. I found a previous E2E post that…
Part Number: SN6505B Other Parts Discussed in Thread: SN6507
Tool/software:
Hello,
I need an isolated 24VDC power supply (50mA minimum) that is generated from the 5VDC.
Can I use a SN6505B with a transformer flipped 180°: 750319694 or 750317828 or 750316856…
Part Number: SN6505B Tool/software: Hi sir
I need to design a isolator power, vin is 5v , vout is 15v, may I know the max output current in second side?
if i need a +/-15V when vin is 5v, may i know the max current output?
thanks
Part Number: SN6505B-Q1 Tool/software: Hello,
I am considering using SN6505B-Q1 isolator driver for power isolation in ECG board.
I have several questions:
Can you please review my circuit for supplying isolated 3.3v :
The transformers considered here…
Part Number: SN6505B Tool/software: Dear Experts,
I would like to inquire about how to estimate the power consumption and temperature rise data of SN6505. Currently, our application scenario is used in the isolated drive power supply of photovoltaic…
Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6505A-Q1 , SN6505A , SN6505B , SN6505D Tool/software: Hello,
I would like to use SN6505B-Q1 for isolating power for ECG use. I would like to know:
1. What is the difference between SN6505A-Q1…
Part Number: SN6505B Tool/software: Hello,
I'm trying to get a soft-start time of around 1ms with an SN6505B to synchronise with an SN6051 + LDO with 1ms soft-start. According to the data sheet, with a load capacitance of 40uF, the start-up time is approximately…
Hi Nilesh,
Thank you for sharing the block diagram connection between SN6505B, ADCs and the line voltages, this helps me understand the power supply connections better and now, I don't have any concerns in the connections between SN6505B and line voltages…
Part Number: SN6505B-Q1 Tool/software: hi expert
i saw the following parameter in datasheet.
my question is that whether is this function disable during soft-start stage?
thanks
Part Number: SN6505B Hello,
We're working with the SN6505B and over-loading the output to see the behavior in the system.
What we are observing is the output voltage start to hiccup after about 1 second in overload condition.
Then output hiccup occurs…