Part Number: SN6505B-Q1 Other Parts Discussed in Thread: SN6501-Q1 , SN6505A-Q1 Hi, can you advice me with a better part for EMC performance than SN6505B-Q1? Today I'm using this part for the push-pull converter of insulated gate driver power supply, but…
Part Number: SN6505B Other Parts Discussed in Thread: TPS7A05 , SN6505A Hi,
We have to power supply a 4 channels isolated data acquisition system and we are looking for an ultra low-power isolated DC-DC converter with the following specs:
VIN: from a 3…
Hi Andrew, Can you please provide SN6505B-Q1 IC, internal MOSFET information i.e., gate charge, rise and fall time as soon as possible, as it was currently unavailable. Kind regards, Vamsi Bankuru
Part Number: SN6505B Other Parts Discussed in Thread: SN6501 , , SN6507 Hi team,
Recently my customer is evaluating SN6501 and SN6505B, some questions about protection and safety came up. Could you pls help with these questions? Thanks a lot!
SN6505B:
…
Part Number: SN6505B-Q1 I want to confirm if it is ok that I design for output higher than 30V, like 31V?
If not ok , what limits the output, the internal MOSFET?
Part Number: SN6505B
Customer has built product giving the SN6505 5V supply, whilst providing the enable pin 3.3V.
Customer is trying to determine how much exposure they have with this setup.
What is the typical multiplier for the enable? (0.55x?)
What…
Hi Cedric,
I didn't hear back from you in a while, I am hoping that you were able to test a transformer with lower leakage inductance and avoid the ringing / transients. I will go ahead and mark this closed but if you still have questions, please feel…
Part Number: SN6505B Hello, SN6505 can be supplied from 2.5 to 5.5V according to the datasheet and the outputs D1 and D2 are open drain outputs. This should make it possible to supply the device with a voltage of e.g. 3.3V while supplying the center tap…
Part Number: SN6505B Hi team,
Can 78253/35JC be used for the SN6505B transformer?
It is compatible for the MAX253. https://www.murata.com/en-global/products/productdetail?partno=78253%2F35JC
The input voltage is 3.3V, a LDO is used after isolation and…