Part Number: SN6507-Q1 Other Parts Discussed in Thread: LM317 , SN6507 Hi team, we are observing this 68v peak.Could you please advise us on ow to resolve this issue
w
Part Number: SN6507 Hello Team,
I'm an intern, trying to use the SN6507 to stabilize a variable input (between 18-30V with 24V nominal) to 24V. The only problem is that my setup is pulling a lot of amps (2A+). I have found this problem in both real…
Part Number: SN6507 Hi,
I am working on a circuit with 24V to 24V isolation using SN6507 and Würth Elektronik 750319697 transformer. I am seeing both parts get very warm even under idle condition with minimal current draw. The parts are getting to about…
Part Number: SN6507 Dear costumer support.
I am an intern trying to use the SN6507 with the Würth 750320325 transformer for 24V-->3.3V. It is for a wide ranging input between 18V and 30V, with 24V nominal. If I am understanding the datasheet well, the…
Part Number: SN6507 I am interested in the SN6507 because it has a variable clock freq. and has spread sprectum to reduce EMI. There is a figure to derive clock frequency by a resistor value. Figure 8-6 is hard to read accuractly between a frequency of…
Part Number: SN6507 Hello,
I am working on a design of a push-pull converter for generating from an input voltage of 24V (+-6V) an isolated 5V / 2W for a stepper motor servo drive. The design should take the variation of the input voltage into account…
Part Number: SN6507 Hi, Is it difficult to exceed 0.5A on output current under SN6507 push-pull isolation configuration?
My customer wants to implement the following.
Input : 24V +-10% Isolated Output : 24V Isolated Output current : 550mA
Webench…
Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6507 Hi TI E2E team,
For the SN6507 (VCC = 12–21V), what is the best/recommended way to drive the EN/UVLO pin from a 3.3V PIC GPIO so it is safe for any power-up sequence (e.g., PIC up while…
Part Number: SN6507 Hi Team,
I am working on worst case analysis of SN6507 push pull transformer driver. I need information regarding MOSFET's used inside IC.
Could you provide me the MOSFET part number to know Rds value at diff temperatures (-40…
Part Number: SN6507 Hi Team,
Could you let me know the max. allowed load current.
and could you share me any application note which provides both positive and negative outputs.
Do you have any worst case calculations for this IC ?
Thank you…