Part Number: SN6507 Tool/software: The switching frequency parameter of the SN6507 as described in the datasheet, is that the double frequency of what you get on each of the SW1/2 outputs?
I am asking as I am going to replace an old ISL6744 circuit…
Part Number: SN6507 Tool/software: Hi Team,
I am currently using SN6505, in conjunction with a 760390015(datasheet recommended) which has a 1:2 turn ratio. Can i use the same transformer with the SN6507 driver. My reason to switch from SN6505 to SN6507…
Part Number: SN6507 Tool/software: Hi TI Team
I have a question regarding R_ILIM with the SN6507. I have an EVAL-board from WE and have tested a few different parts here and there. The only thing I don't understand is the R_ILIM. I used a 68k resistor…
Part Number: SN6507 Tool/software: Dear Teams,
I use SN6507 to design an isolated power supply with an input voltage of 5V, an output voltage of 15V, and an output current of 200mA.
Do you have a recommended transformer?
Thanks & Best regards.
Part Number: SN6507 Tool/software: Hi team,
The datasheet states "Note that it's recommended that VCC pin powers up before CLK pin.". While, is there any limitation for power-down sequence between VCC and CLK?
Just to make sure, is there no sequence…
Part Number: SN6507-Q1 Tool/software: Dears,
May I ask if the Wurth series of transformers equipped with SN6507-q1 can support a switching frequency of 1MHz?
Part Number: SN6507 Other Parts Discussed in Thread: UCC14141-Q1 Tool/software: Hi,
We are using SN6507 in our design and need UL certificate/IEC certificate in the deign.
Regards,
Mayur
Part Number: SN6507-Q1 Other Parts Discussed in Thread: SN6507 Tool/software: Hello team,
Could you please share pspice model for the part SN6507-Q1 for transient analysis?
Thank you,
Part Number: SN6507 Tool/software: Hello,
We have developed in Isolated power supply sch using SN6507.
During testing, we found IC and TXR temperature are increasing 50+ Degree.
Below is snapshot of SCH, output of this power schematics will drive…