Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Part Number: SN65C1168E Hi, Team .
could you see below?
1. the spice model spec depends on the power supply and load ?
2.in order to get the more real result, should customer re-change the spice model internal spec ?
3.which sentence can customer change…
Part Number: SN65C1168E Other Parts Discussed in Thread: ISO3086 Hi, staff
Communication between SN65C1168E (Tx)-ISO3086 (Rx) stops. Once communication stops, it will not resume until you replace the device. This means that the device has been corrupted…
Part Number: SN65C1168E Hello,
I'm going to design the SN65C1168ERGYR footprint, but I think there's a error in its datasheet on page 24 ( www.ti.com/.../sn65c1168e.pdf): in the last row we can find " Package complies to JEDEC MO-241 variation…
Part Number: SN65C1168E Hi, Team,
This is MASA.
Could you tell me below?
Is SN65C1168E's input impedance same as realistic situation and simulation situation?
the reason why I asked is below.
1 Customer had converted out SPICE model into LT spice…
Part Number: SN65C1168E-SEP Greetings!
My customer has the following questions about the SN65C1168EMPWSEP:
If one of the drivers and/or receivers fails, is the other one isolated enough that it will still function?
Are there specific failure modes where…
There are RS-232 transceivers that need external high-voltage supplies, e.g., SN75155.
But in practice, high-noise environments are much easier handled with differential signals like LVDS (e.g., SN65LVDS049) or RS-422/RS-485 (e.g., SN65C1168E or 2× THVD1512…
Part Number: SN65C1168E Hi,
Kindly provide below details for Part# SN65C1168E
Maximum Cable length SN65C1168E can operate.
How many SN65C1168E nodes will be connected on RS485 bus.
Part Number: SN65C1168E Hello,
Our customer use the SN65C1168E.
The customer don't use the DE function.
Is it possible to connect the DE terminal to VCC directly?
Best Regards,
Naoki Aoyama
Part Number: SN65C1168E Hi All
My customer is using SN65C1168E for their 2ch RS422. Then, they'd like to use same device for their 1ch RS422 too.
When they don't use the second driver and receiver of SN65C1168E, how should they handle terminals…