Part Number: SN65DSI85 1. Does SN65DSI85 support a compressed video (DSC) pass-thru? When I tested it, it didn't work. I think SN65DSI85 checks data type in packet header if it's 0x3E or 0x0B. Is it correct?
2. If question 1 is right, is there any…
Part Number: SN65DSI85 Hello,
Does SN65DSI85 support to connect two panels with dual link mode? If yes, does it mean each panel's resolution is the half of the original resolution?
Best regards
kailyn
Part Number: SN65DSI85-Q1 Other Parts Discussed in Thread: SN65DSI84-Q1 , SN65DSI84 Hi experts,
Customer want to change SN65DSI85-Q1 to SN65DSI84-Q1, can they replace the chip directly on PCB? Any hardware change is needed? For software, which registers…
Part Number: SN65DSI85-Q1 Hello team,
Could you pls let me know Tvcc requirement for power up sequence??
I understand Ten should be 1ms as table below. but it is for max value. so EN should be high after 1ms of VCC rise??
Thank you.
Part Number: SN65DSI85-Q1 Hello Team,
My customer is asking how to use INT of device.
Before go to customer, I want to make sure with you my understanding.
Could you pls help answer several questions as below??
1) How to enable DSI_IRQ?? …
Part Number: SN65DSI85 Hello team,
This question is related to the following question.
e2e.ti.com/.../4004899
The customer has changed only the data line of the SN65DSI85ZQER as follows and it does not work.
I think I see no problem with section…
Part Number: SN65DSI85 Hi team,
My customer would like to ask two question.
Can we use the 2.5~3.3V external SSXO for DSI85 CLK pin? I see the max voltage is 2.175. so they can't use 2.5V to 3.3V right?
If there any configuration about the Frequency…
Part Number: SN65DSI85 Dears
Is there a simulation model for SN65DSI85?
I want to logically verify whether DSI connection with SN65DSI85 is possible and LVDS output is possible. Is there a model that can be simulated such as vhdl or verilog model…
Part Number: SN65DSI85 Hello team,
Is it possible to connect data signals in this way?
DSI-D3-P――――― DA2P A_Y2P ―――――A-Y3P DSI-D3-N――――― DA2N A_Y2N ―――――A-Y3N DSI-D2-P――――― DA1P A_Y1P ―――――A-Y2P DSI-D2-N――――― DA1N A_Y1N ―――――A-Y2N DSI-D1-P…