Part Number: SN65HVD230 Hi there, are there any possible issues with having one upstream SN65HVD230 running at 5V, while other CAN nodes with SN65HVD230 are running at 3.3V? Any potential backfeeding issues? Or does the transceiver know to use the correct…
Part Number: SN65HVD230 Other Parts Discussed in Thread: TCAN334 , Hello, can multiple non-isolated SN65HVD230D CAN XCVRs be used with an upstream isolated CAN XCVR without any issues? I am currently experiencing an issue where there is coupled switching…
Part Number: SN65HVD230 I have been using the SN65HVD230 successfully for several years now, on some of the latest run of prototype boards (only 42 built) the xcvr is behaving very strangely. In the circuit, vref is tied to the contacts of two solid state…
Part Number: SN65HVD230 Other Parts Discussed in Thread: SN65HVD251 , Because of the SN65HVD230 has shortage issue, so some of device need to change the CAN to SN65HVD251.
If one side we use SN65HVD230(VCC is 3V ~3.6V) and the other side is SN65HVD251(VCC…
Part Number: SN65HVD230 Hi,
We have used CAN SN65HVD230 in our Vehicle Tracking Device board. Testing is done in Lab, using a CAN to USB convertor and a PC. Worked fine. We are facing lot of failures of CAN IC in multiple vehicles which
consist of multiple…
Part Number: SN65HVD230 Hi,
I am using a 3.3V sn65hvd230 with ESP32 MCU. I have programmed MCU to transmit frames continuously. Initially, everything is ok but after a day CAN bus hangs Up. Voltages of CANL , CANH are 2.25V and 2.25 Volts.
respective…
Part Number: SN65HVD230 Hello Team,
My customer originally used the device SN65HVD230DR, unfortunately, that's no longer in stock. However, they found alternatives such as "SN65HVD230MDREP" and "SN65HVD230QDG4Q1".
The datasheets…
Part Number: SN65HVD230 Attached below is the schematic of how we used it. The SN65HVD230D corrupts CAN line signals, it works again after replacing it with a new one. Multiple of our boards are experiencing the same problem.
^Here's a screenshot…
Part Number: SN65HVD230 Hi,
We are using the SN65HVD230DR as a CAN bus transceiver on a BLDC motor controller. We are facing multiple controller units with the SN65HVD230DR out of order. Most of them are externally fine but do not work anymore. One presents…
Part Number: SN65HVD230 We have used CAN SN65HVD230 in our BMS board. Testing is done in Lab, using a CAN to USB convertor and a PC. Worked fine.
Product is in pilot production now. We are seeing lot of failures of CAN IC.
Please review my schematic and…