Other Parts Discussed in Thread: SN65HVD257 Hello
I would like to use sn65hvd257 powered by 5v , but my MCU is powered by 3.3v ; I could not understand that from the datasheet , what is minimum volt for logic high and low for the TXD ?
Thanks
Part Number: TCAN1145-Q1 Other Parts Discussed in Thread: SN65HVD257 , Hello,
1. We have this part no "SN65HVD257" which is having functional safety features .Is that means it is functional safety compliant ?
2. Is this CAN transceiver "TCAN1145-Q1…
Part Number: TCAN330 Other Parts Discussed in Thread: SN65HVD257 , TCAN337 Hi,
I am currently using CAN transceiver "SN65HVD257" in my design for redundant multi topology CAN network.
1. Can " TCAN337" be used as an alternate ? (difference in voltage…
Part Number: SN65HVD234 Other Parts Discussed in Thread: SN65HVD257
Hi guys.
I have the CAN transceiver SN65HVD234 on my device (in some application I used SN65HVD257 instead of SN65HVD234).
The two pins CANH and CANL are protected from ESD events…
Hi Atsushi,
CAN bus fault detection is limited for 8-pin CAN transceivers. Most applications today are implementing I/O voltage shifting for the extra pin feature. The SN65HVD257 device is a 5V CAN transceiver with a FAULT output. This FAULT pin will…
Thanks Sir. Also, Can you throw some light on "The SN65HVD257 CAN EVM also provides PCB footprints for different bus terminations, bus filtering, and protection concepts." What is the significance of PCB footprints and what is bus filtering? Could you…
Bob,
Thanks for your message. I have "SN65HVD257 CAN EVM" which has two CAN transceivers. Can I use EK-TM4C123GXL with SN65HVD257 CAN EVM?
Don't you think C2000 series is better for my case?
For CAN transceivers,
I found three CAN transceivers EVM: TCAN10XX, SN65HDV255 and SN65HVD257 where the later EVM comes with two SN65HVD257 which is suitable for set up in a redundant configuration. The one that's used in LAUNCHPAD is SN65HVD234D which…
Part Number: TMS320F28069M Other Parts Discussed in Thread: SN65HVD257 , SN65HVD33 Hi,
My project is going to get finished and I would like to have a PCB board designed based on TMSF28069M MCU. I need to have the following components on the board: …
Other Parts Discussed in Thread: SN65HVD257 Dear all,
In a safety application we are using SN65HVD257 CAN drivers in a Redundant Physical Layer CAN Network Topology as indicated in the relevant data sheet (see figure attached). The number of our nodes…