Part Number: SN65HVD3082E Other Parts Discussed in Thread: SN65HVD3088E , SN65HVD3085E Hi team,
I have a few questions regarding SN65HVD308xE. As a quick note, I've been referencing Section 6.7, Figure 2 and Figure 5 of the datasheet and this e2e t…
Part Number: SN65HVD3082E Tool/software: Code Composer Studio This components in SMD version SN65HVD3082ED is marking in first line VP3082, in second line there are different code
65M, 67M, 49M and other. What is this different code?
Thanks
Best regar…
Part Number: SN65HVD3082E Hello team,
When I was testing the threshold parameter of the reciever refering to the datasheet, two methods were used and their results are different.
The first method is adding a squarewave directly to the two input pins…
Part Number: SN65HVD3082E Hi
I would like to know about bias resistor of the external fail-safe circuit such as the following circuit.
We should choose the resistor(above R) to be more than 200mV between A and B. Is my understanding correct?
If it correct…
Part Number: SN65HVD3082E Hello, customer did the performance comparison between SN65HVD3082EDR and MAX1483ESA+T. They found the behavior is a little different on the RS485 output in the biginging of voltage level.
RS485IC_Compare_20181210 (2).docx
…
Part Number: SN65HVD3082E Other Parts Discussed in Thread: THVD1450 , THVD1429 I need to design repeater for MVB (Multi Function Vehicle Bus) for ESD mode.
As it is based on RS 485 logical levels, i am thinking of using RS 485 trans receiver.
My application…
Part Number: SN65HVD3082E Other Parts Discussed in Thread: THVD1550 , THVD1500 , THVD1450 Hi
I has a product use SN65HVD3082E but we test EMI when 2M~20M is too high, do TI has any idea can help.
wave as attachment.
Part Number: SN65HVD3082E Other Parts Discussed in Thread: SN65LBC184 Hi Team,
Here is south China FAE Sunny, we meet a SN65HVD3082E communication problem, customer use SN65HVD3082E communicate with USB 485 debuger, the wire is only 1 meter, the SN65HVD3082E…
Part Number: SN65HVD3082E Hi
Does SN65HVD3082ED have certificates like UL or VDE certification? Can you send it to my Email : jerry.hsueh@wpi-group.com
thank you
Part Number: SN65HVD3082E Good day Colleagues,
Could you tell me about a total power consumption of the SN65HVD3082E for 100kBit/sec data rate and 256 loads? Termination is 60 Ohm.
Am I correct the total current will be 35 mA + 8 mA = 43mA (figures 5…