Part Number: SN65HVD3088E Dear TI Team
What is the impedance value between pin A and pin B (between pin No. 6 and pin No. 7) of SN65HVD3088EDRG4? (The reference value is fine, so I'd be happy if you could tell me.)
Best Regards, Y.Ottey
Part Number: SN65HVD3088E Hi Team,
Kindly let me know the receiver output maximum rise and fall time of SN65HVD3088E. In datasheet it is shows as 3ns. But when I'm testing it is up to 5ns is showing. Kindly reply.
Warm regards,
Monisha OM
Part Number: SN65HVD3088E Hi, My customer has the following questions. Please answer it.
Termination resistance RL that determines the differential output voltage
(1) In the circuit shown in your data sheet Figure 8, the differential output voltage is…
Part Number: SN65HVD3088E Hi Experts,
My customer wants to estimate the power consumption so they are asking about the maximum of Vod.
Do we have any data for max Vod at RL is 54 ohm?
Regards,
Uchikoshi
Part Number: SN65HVD3088E Dear TI Team
I would like to ask about SN65HVD3088E
Is it okay if a voltage (5V or less) is applied to the A and B terminals of the SN65HVD3088E when Vcc = 0V (when the power is off)? (If you check the maximum rating, it is stated…
Hi Yanagisawa-san,
RS-485 standard allows 32 unit loads on the bus - The SN75ALS181 is a 1 unit load device so up to 32 SN75ALS181 on one bus, but the SN65HVD3088E is 1/8th unit load so you can place up to 256 nodes on one bus with the SN65HVD3088E. …
Part Number: SN65HVD3088E I have a customer requesting hysteresis info for the D, DE and REbar pins.
Can someone provide me with this?
Thanks.
Regards, Darren
Part Number: SN75ALS181 Other Parts Discussed in Thread: SN65HVD3088E ,
Is there any problem with the following connections for "SN75ALS181NSR"?
We are considering replacing the SN75ALS181NSR with the SN65HVD3088ENSR.
Number of nodes: 64
Communication…
Hi Jimmy,
So beyond speed and ESD ratings there are a few other key distinguishing factors:
1. THVD1550 can handle a higher temperature range: -40C to 125C instead of -40C to 85C that the SN65HVD3088E is spec'd as.
2. THVD1550 has higher fault protection…
Part Number: SN65HVD3088E Hi experts,
My customer asks Hot-Swap function of SN65HVD3088E.
Could you tell me if SN65HVD3088E has Hot-Swap function or not?
Thank you.
Best Regards,
Atsushi Saito