Part Number: SN65HVD62 Hi,
I want to use several SN65HVD62's on a 24V bus, not the normal use case but.. This should be possible since the usage of DC blocking capacitors.
This bus contains of one master and several slaves.
1. Where can I find information…
Part Number: SN65HVD62 Hi Team,
Our customer tries the OOK loop. install JU13. And input +3dB OOK signal at point 1. Test the output OOK signal at point 2.
They found the output signal amplitude is only 887mV(nearly -3dB). That is to say, after this loop…
Part Number: SN65HVD62 Hi Dear expert,
May I know what is the requirement of Xtal pin 14 and 15 duty cycle requirement?
Thanks a lot for your reply in advance.
Joyce
Part Number: SN65HVD63 Other Parts Discussed in Thread: SN65HVD62 Tool/software: Here is some questions from customer side:
I want to double confirm the meaning of “maximum level” spec in below table. Is it mean that the maximum remaining interface…
Part Number: SN65HVD62 Hi;
The datasheet of SN65HVD62 described that SN65HVD62 modulate and demodulate signals between the logic (baseband) and a frequency suitable for long coaxial media. But how long of the coaxial of SN65HVD62 could support?
Best re…
Part Number: SN65HVD62 Hello.
I use the SN65HVD62 on the project TMA.
If I don't use the RS485, I want to connect the SN65HVD62 with the MCU directly. is it reliable ?
Because the pin5(DIR) of SN65HVD62 is out, Can it be floating ? I can't find the pin5…
Part Number: SN65HVD62 Dear Sirs,
My customer asked us about DC power line of SN65HVD62
System architecture assumes that External Battery Backup Unit is connected to main system with only power supply cable which also serves as communication media. Data…
Part Number: SN65HVD62 Hi Sirs, Would you pls advise if the SN65HVD62 support On/Off Keying (OOK) on 2.6MHz carrier, ON=logical zero? Thank you and Best regards, Wayne Chen 03/30/2017
Part Number: SN65HVD62 Other Parts Discussed in Thread: AFE031 Hi Sirs, Would you please advise of the AFE031 and SN65HVD62 support customer's requirements below? Physical serial communication, OOK modulator & demodulator that carried on DC Power Line…
Part Number: SN65HVD62 Hi,
I'm confirming the schematic of SN65HVD62EVM. Please let me know the reason why C6/470pF and L1/0.22uF are used. We couldn't use the same parameter for these capacitance..
Best Regards,
Toshiyuki