Part Number: SN65HVD73 Other Parts Discussed in Thread: SN65HVD70 Hello,
we are using the SN65HVD73 transceiver with an UART input. The baudrate of the UART port is quite low (115200) and the cable length also short (<5m), so i thought we won't need any…
Part Number: SN65HVD73 Other Parts Discussed in Thread: SN65HVD1473 , The delivery time of SN65HVD73DGS is getting longer and I cannot get it by the desired delivery date, so I am looking for a replacement.
SN65HVD1473DGS seems to be available, but I can…
Part Number: SN65HVD73 Other Parts Discussed in Thread: THVD1424 SN65HVD7x supply voltage use 2.5V.
WE use vcc2.5v can work normally. I want to know the risk of using it on 2.5v
Part Number: SN65HVD73 Hi,
In datasheet of SN65HVD73DR, in Pin configuration and functions section, Data signals are described as 'Digital bus output Y', 'Digital bus output Z', 'Digital bus input B' and 'Digital bus input …
Part Number: SN65HVD73 Hi,
In datasheet of SN65HVD73DR, section Detailed Design Procedure, there is one pull up is given to RX pin in the diagram. But in any other section of datasheet does not say anything about this.
Why this pull up is required? If processor…
Part Number: SN65HVD73 Other Parts Discussed in Thread: PROFIBUS Hi,
We are planning to use SN65HVD73DR in our design.
Our requirement is that our system has to work in both half duplex and full duplex mode. We planned like below,
Full duplex: Normal full…
Part Number: SN65HVD73 Hello team,
There is the difference between fig37 and fig41 for placing termination resistor.
I believe SN65HVD73 should be placed termination resistor at both Tx and RX. Is my understanding correct ?
And termination resistor should…
Part Number: SN65HVD73 Hi ,
the customer use SN65HVD73 for full-duplex change to half-duplex mode, but the output signal always had high level of 0.68v, what caused it?
schematic as below:
Part Number: SN65HVD73 Hi Tiers,
The customer is using SN65HVD73 for their previous version and they want to change from Full-Duplex to Half-Duplex.
Could SN65HVD73 achieve Half-Duplex?
If yes, could you provide the reference schematic?
Thanks and best regards…