Part Number: SN65HVD73 Hi Tiers,
The customer is using SN65HVD73 for their previous version and they want to change from Full-Duplex to Half-Duplex.
Could SN65HVD73 achieve Half-Duplex?
If yes, could you provide the reference schematic?
Thanks…
Part Number: SN65HVD73 Hi Team,
We are planing to use this SN65HVD73 for RS485 .
They are two differential Paris signal can please suggest how much impedance need maintain this two differential paris
If possible plz share the Layout guideline for…
Part Number: SN65HVD73 I’d like to replace from ADM3076EARZ to SN65HVD73D.
Both packages are same SOIC-14, however according to data sheet, 13pin of TI is VCC and 13pin of ADI is NC.
Is it possible to be NC on 13pin of SN65HVD73D?
Best Regards …
Part Number: SN65HVD73 Other Parts Discussed in Thread: SN65C1167E , SN65C1168E , THVD1452 , SN65HVD72 Hi
Our customer are looking for Dual and Full duplex device. And it's also supported 3.3V supply.
SN65HVD73 is single channel. Do you have dual…
Part Number: SN65HVD73 Hi ,
I wanted to know the max current consumption for the SN65HVD73 part where my UART speed is 5Mbps Max.
I also wanted to know how the cable properties will affect the signal and power consumption factors of the device ? …
Part Number: SN65HVD73
Hello TI,
Similar to this thread:
http://e2e.ti.com/support/interface/f/138/t/353743
we wish to extend the SE input swing of the SN65HVD7x buffer to be RS-232 swing compatible: ±25V if possible, or at least ±15V, per input…
Part Number: SN65HVD73 Hi
I have some question regarding the external fail safe circuit.
Do we need the external fail-safe circuit for the differential input when it is in the communication stop and line open?
And how much the internal resistor…
Part Number: SN65HVD73 I'm working on an embedded Linux system that uses an off-the-shelf computer-on-module (COM) with a custom "baseboard" (I/O breakout and power regulation).
Our baseboard has two differential serial (RS-422) ports using the SN65HVD73…
Other Parts Discussed in Thread: SN65HVD73 Dear, All
A customer has been designed using the SN65HVD73. They may want to know about the Receiver Inputs circuit of SN65HVD73. They want to adjust the voltage of the failsafe. Please tell me the resistance…
Part Number: SN65HVD70 Other Parts Discussed in Thread: SN65HVD73 , THVD1410 Hi,
We are using RS485 SN65HVD70, My doubt is, when the Termination resistor(Rt) and Bias resistor's are mandatory or optional ?
We read document TIA/EIA-485 (RS-485),…