Part Number: SN65HVD75 Hello,
I would try a pin reduced approach to sharing a signal for DE/RE# and another for D/R.
Provided that controller will have to change direction of port for D/R signal with proper timing avoiding contention with R, could…
Part Number: SN65HVD75 Other Parts Discussed in Thread: PROFIBUS , SN74LVC1G123 , SN74LV123A , SN65HVD3082E Hello,
We would like to have carrier detect signal from RX data (we use RS485 half duplex and fieldbus 1 Mbits like Profibus). In fact we would…
Part Number: SN65HVD75 Other Parts Discussed in Thread: SN65HVD11 Will part # SN65HVD75 fit the same footprint as part # SN65HVD11?
If not, can you point me to compatible part numbers where we do not have to change footprint?
Thanks
Hi,
I don't think CPDQC12VE-HF is suitable here since its 19~23V clamping voltage is higher than the abs max of SN65HVD75 (-13V/16.5V). If you want to have better ESD level, you may want to consider SM712 .
Regards,
Hao
Part Number: SN65HVD75 Other Parts Discussed in Thread: THVD1450 Will there be any problems when using SN65HVD75 to design an automatic RS485 transceiver circuit?
Part Number: SN65HVD75 Other Parts Discussed in Thread: SN65HVD3088E , THVD1550
Hi team,
Is DS1487 EOL?
Could you kindly suggest DS1487 alternative?
I recognize SN65HVD75, but it would be better if any other alternative which supports 5V input…
Part Number: SN65HVD75 Dears:
as above figure12&13,it is all TX direction, Figure 12 is easy to know,the timing is signal in to differential out ; however, in figure13, is it signal in to out port timing ?
what is the mean "driver enable and disable…
Part Number: SN65HVD75 Hi Team,
Can you help confirm if SN65HVD75 can work long time when the logic input at D pin is 5V while the power supply at Vcc is 3.3V?
The fist page of datasheet says"5-V Tolerant Logic Inputs Compatible With 3.3-V or 5-V…
Part Number: SN65HVD75 Dear :
I have one product with RS485 SN65HVD75DGKR to do withstand voltage test, but I found the leakage current is 11mA above, standard request is below 10mA,so I need you help to give me suggestion.
test condition: The A/B…