The SN65LVDS3486 is an LVDS receiver.
How many channels do you need? For one channel, use a fast transceiver like the SN65HVD78 or SN65HVD10. (The THVD1450 is more modern, but has larger skew.)
Other Parts Discussed in Thread: SN65HVD78 , SN65HVD75 Hello,
We need data transmission rate upto 20msps and we need a transmission line length of 60-70meters with cat6 cable. The appropriate ic seems to be sn65hvd75. However, we have many sn65hvd78 with…
Other Parts Discussed in Thread: SN65HVD78 Hello all,
In my project, i use sn65hvd78 rs485 tranciever to transmit and receive 15mhz clock and data signals. I use one sn65hvd78 to transmit and one for receive. I use a 5 meter CAT5 cable. The problem is…
Part Number: SN65HVD08 Other Parts Discussed in Thread: SN65HVD78 , Dear TI,
I want to know about difference between SN65HVD08D and SN65HVD78DR.
Thank you
Best Regards,
Inho Jeon
Hi Asier,
We do have a few options that hit the same signal speed or higher, but they typically do have a bit more features than this part such as higher protection ratings.
The THVD1450 is a p in-to-pin device that offers integrated IEC ESD protection…
Part Number: SN65HVD82 Other Parts Discussed in Thread: THVD1510 , SN65HVD888 Team,
Could HVD888 be used instead of HVD82? Are they P2P dropped-in replacement? SN65HVD888 vs SN65HVD82 If not is there a way to make a PCB change to accommodate the use of…
daejin,
When you did the measurement, was the device powered up with a 5V supply? What's voltage on the input (pin 1)?
FYI - you can find the driver's equivalent schematic on the other RS485/422 devices, like this one of SN65HVD78 (Figure 18 on…
Part Number: THVD1450 Other Parts Discussed in Thread: SN65HVD72 , SN65HVD75 , SN65HVD78 , THVD1410 , , SN65MLVD204B , SN65HVD23 Hi;
I'm working on a project, which based on RS485 / RS422 peer to peer connection, with 30' UL2919 cable (12.5 pF/ft) in between…
Jim,
If data rate is low, the major limitation on the communication distance is DC loss, like how you calculated. If data rate is high (in Mbps), the main loss comes from high frequency. Please check out the 'Cable Length vs Data Rate' plot (Figure 21…