That diode doesn't break down until ~32 V, so depending on the current it needs to sink the peak clamping voltage might be higher than the absolute maximum limit of the SN65HVD96. You may want to double-check that and then see if some additional current…
Divyanshu,
I agree that would be ideal, but I've checked to see if these part number were noted anywhere outside of the published document but I haven't been able to locate any information. Since this work was performed several years ago, I think this…
Part Number: SN65HVD96 Hi,
We are developing new product based on SN65HVD96 and Power over data application note http://www.ti.com/lit/an/slla336/slla336.pdf?&ts=1588921006385 and it's not working.
We have based our design in the one in Figure5. …
Part Number: SN65HVD96 Other Parts Discussed in Thread: THVD1520 , THVD1419
Dear all:
I used SN65HVD96DR chip, the circuit principle is as follows, but I tried 5pcs samples, but they could not communicate.Change for MAX485 can normal communication…
Part Number: SN65HVD96EVM Other Parts Discussed in Thread: SN65HVD96 , TIDA-01171 Hello everyone,
I am working on SN68HVD96 EVM in order to send power over Data Through RS485.
I have a question about the bellow figure mentioned in the datasheet (…
Part Number: SN65HVD96 We are trying to power a device with around 25v and 40amp of power. The data would be send from the power source to the the sink(motors).
Does this require the inductors on the power source side for this to work ? I could not…
Part Number: SN65HVD1786 hello,
I am working on the Power over Line which couples data and power over 2 cables. Bellow the schematic of the intended circuit which includes the SN65HVD1876 RS485.
In fact, the idea is to power the RS485 in the reception…
Part Number: SN65HVD96 Hi
I am developing a solution for Powerline communication. Study different Circuits, I stuck when I send a signal from USB to rs485 Converter to my module it is not read any data on the slave side . when I check with MSO I find…
Part Number: SN65HVD96 Other Parts Discussed in Thread: TIDA-00527 , RE:
TI Designs: TIDA-00527 RS-485 Power Over Bus
SN65HVD96
Hi,
Could you please provide details of the maximum distance, power and the data rate achieved with your example of…
Part Number: SN65HVD96 Hello,
Based on this application note "slla336" we're willing to design power over data communication bus with maximum number of nodes.
Known parameters: +12V DC bus, 20kbps maximum bitrate
Unknown parameters:
- Maximum…