Part Number: SN65HVDA100-Q1 Hello,
We want to use this interface in a tester to test the unit which has LIN interface.
In our board, we are planning to interface this IC via UART to the Banana Pro board which runs on Linux.
Please let me know, is it…
Part Number: SN65HVDA100-Q1 Other Parts Discussed in Thread: SN65HVDA100 , TLIN1029-Q1 Hi team,
I want to know if SN65HVDA100 can replace TJA1021? is it the best one?
my customer also use UJA1023 in there current project, do we have device can replace?
thank…
Part Number: SN65HVDA100-Q1 Other Parts Discussed in Thread: SN65HVDA100 Tool/software: Linux Hi,
We would like to configure "SN65HVDA100-Q1" as LIN master mode and get end sensor data. The connections are [TI TUSB4041 ==> (USB->UART Bridge)…
Part Number: SN65HVDA100-Q1 Other Parts Discussed in Thread: SN65HVDA100 We are working on some existing EOL tester and NCV7321D11R2G is used for LIN functionality
Can we drop-in replace this IC with TI part# SN65HVDA100QDRQ1?
Part Number: SN65HVD255DEVM Hello,
Does the SN65HVD255D Evaluation Module can work with a SN65HVDA100-Q1 instead?
If not what dev board would you recommend to evaluate LIN with a AM335X?
Thanks.
Part Number: SN65HVDA100-Q1 Hi Champs,
My customer wants to know Rds_on max value of RXD open drain FET, to evaluate worst case of VOL.
In the datasheet IOL_min of RXD is specified as 3.5mA with the condition of "LIN=0V, RXD=0.4V".
If IOL is…
Thanks for quick response.
Ok. So will SN65HVDA100-Q1 , as a LIN 2.1 master node, handle LIN 2.0 slave node? OR Does SN65HVDA100-Q1 , as a LIN master node, have all the functionality of LIN 2.0 master node to handle LIN 2.0 slave node?
Thanks
Part Number: SN65HVDA100-Q1 Hi,
I am a bit confused by the INH pin of the device. Every diagram I see with SN65 shows INH directly connected to the EN of the LDO but the block diagram makes it look like that wouldn't work to disable the LDO unless there…
Part Number: TCAN1043-Q1 Other Parts Discussed in Thread: SN65HVDA100 , TCAN1043 Hi Champs,
My customer monitored unexpected behavior in INH of both TCAN1043 and SN65HVDA100, as shown in attached file.
Could you check and answer for the question?
In parallel…
Yusuke-san,
I apologize. I was unable to test the SN65HVDA100-Q1 today as promised. Time will be set aside tomorrow to finish the testing. I will also provide details of the test condition.
-Lucas