Part Number: TCAN1044-Q1 Other Parts Discussed in Thread: SN65HVDA540 , TCAN1044A-Q1 , , TCAN1044V Tool/software: Hi Team,
Currently, customer is doing cost down in the new project, so I promote TCAN1044 to replace SN65HVDA540.
But the TCAN1044 will meet…
Part Number: SN65HVDA540-Q1 Other Parts Discussed in Thread: TCAN4550 Is the maximum DS specification for bus Voltage also valid for differential Voltages at CANH / CANL ?
I.e. if CANH=32V & CANL=GND, is device able to withstand ?
If not, what are…
Part Number: SN65HVDA540 Other Parts Discussed in Thread: RM46L852 , TCAN4550-Q1 , RM57L843 Tool/software: Hello, I need to communicate the RM46L852 MCU with 4 independent 250kbps CAN networks. Said MCU has 3 independent CAN controllers, of which one is…
Part Number: SN65HVDA540-Q1 Hello Team,
My customer is looking for a product Low speed CAN transceiver.
They want products with Vcc of 5V and Vio of 3.3V.
So. I will propose SN65HVDA540-Q1.
Does the SN65HVDA540-Q1 support the Low speed CAN standard(ISO11898…
Other Parts Discussed in Thread: SN65HVDA540-Q1 Hi Expert,
I confirmed datasheet of "SN65HVDA540-Q1".
According to this datasheet, user can input 3.3V to VIO and 5V to Vcc.
(Please refer to figure 16 Typical Application Using 3.3-V I/O Voltage…
Hi NIthish,
Please check the VIH in the transceiver datasheet. The VIH is 0.7*5=3.5V which is higher than the MCU I/O output voltage . Like the transceiver output to the MCU to higher than than the MCU VIH. You will need a level shifter.
You can…
Hello McCrea san,
Thank you for your support.
I will propose this reference design.
Can we porpose the SN65HVDA540-Q1 for CAN tranceiver?
The SN65HVD1050 has Silent Mode , however the SN65HVDA540-Q1 has Standby mode.
Thus, we can disable the receiver…
Other Parts Discussed in Thread: SN65HVDA1050A-Q1 , SN65HVDA542-Q1 , SN65HVDA540-Q1 , HVDA551-Q1 Hello ,
I needed some information on CAN in TI piccolo.
1. What are the recommended CAN transceivers for the TI piccolo (28069)?
2. Are there any development…
Other Parts Discussed in Thread: SN65HVD251 , SN65HVDA541-Q1 , SN65HVD255 , SN65HVDA1040A-Q1 , SN65HVDA542-Q1 , SN65HVDA1050A-Q1 , SN65HVDA540-Q1 , SN65HVD257 , SN65HVD256 I was looking at the
SN65HVD1050
and need to know if this supports the SAE J1939.
Hello Sangeetha,
I will need to transfer you over to our TMS320 forum so that they can help you with getting the CAN communication working. But since I support the stand alone tranceivers, I noticed you are using a level shifter and an external transciever…