Part Number: TCAN1044A-Q1 Tool/software: Dear team,
Can we apply VIO which is used for TCAN1044AVDRQ1 to 5pin of TCAN1044ADRQ1? D/S mentions it is NC(=Not internally connected; Devices without VIO).
The background of this query is because my customer…
Part Number: DS90UB935-Q1 Tool/software: Hi,
We are experiencing a loss of video. It happens randomly on one camera. The power up sequence was measured and a register dump was performed of the serializer on the same camera when its OK (streaming) and…
Hello David,
Thank you for confirming the behavior!
--
Regarding *OTP_SPARE* vs. *CUST_MISC*, can we assume that these are functionally identical and interchangeable?
--
Concerning the *factory configuration default*, the documentation describes two cases…
Part Number: LM25180-Q1 Tool/software: PSR Flyback DC/DC Converter Transformer Design for mHEV Applications I n the above link, the design includes transformer design information for 12V output (EP7 core with number of turns, gauge and gap information…
Part Number: TPS57040-Q1 Tool/software: Hello, I would like to send a new IMDS SX000019713 (TPS57040QDGQRQ1, IC) that does not contain the 8.1 classification
Please send to NVision 126016.
Thank you and have a nice day.
Part Number: TPS3704-Q1 Tool/software: Hello experts,
In TPS37042-Q1, there are two NC pins (5/6).
Can 5/6 NC pins be connected to GND in TPS37042-Q1? or is there any concerns for the direct GND connections?
Thanks,
Kento
Hi Chen,
Even if the received frame is less by a byte, this error would be printed. So again, please check the size in the CSIRX and what is received from the sensor. They should exactly match.
and since you are only receiving 2 frames, this print also…
Part Number: ISO7761-Q1 Other Parts Discussed in Thread: ISO7761 , , SN74LVC125A Tool/software: Hello, I designed an SPI circuit using ISO7761 BUFFER as shown in the attached picture.
There are 5 SLAVEs connected to one SPI line. Are there any problems…
Part Number: TXS0108E-Q1 Other Parts Discussed in Thread: TXS0108E
Tool/software:
Hello, I am using the TXS0108E as a level shifter from 3.3V to 5V for my 5 MHz SPI. Unfortunately, I am experiencing unwanted ringing on the edges. To address this, I added…
Part Number: LMQ644A2-Q1 Tool/software: Hi team,
Is it possible to configure this device as single phase 3 or 5 phase (odd number of phases) ?
If the answer is yes and can be used for 5 phases(use 3units of LMQ644A2), do I need to populate LC components…