Part Number: TAS6424E-Q1 Other Parts Discussed in Thread: TAS6424E Hi team,
Could you please advise if all channels are enabled or 1 of 4 channel only enabled for Datasheet Figure 7-5. Output Power vs Supply Voltage?
I would like to drive TAS6424E under…
Part Number: TPS65219-Q1 Hi Team,
For other platforms such as ST Accord 5 (L5964Q), can you recommend more commonly used specifications with stable supply for reference?
(1)VIN range: automotive Vbatt 12V/24V (or low voltage 5V is also acceptable) (2)LDO…
Part Number: TDA4VH-Q1 hi,TI
I'm having issues with eMMC:
1. Unable to switch to eMMC at the uboot command line;
=> mmc list
mmc@4f80000: 0 #eMMC
mmc@4fb0000: 1 #SD card
=> mmc info
unable to select a mode : -5
mmc_init: -524, time 264…
Part Number: LM7480-Q1 Hi Team,
Do we have any test result of LM74xx-Q1 in ISO7637-2 pulse 5b, load dump?
Customer want to see if the pulse is suppressed by LM7480-Q1, how low the Us can decrease.
They wonder if 30V or 26V device can be used after LM7480…
Part Number: DRA821U-Q1 Other Parts Discussed in Thread: DRA821 I'm designing a mixed functional safety + Linux based system for an industrial application. The MCU island on DRA821 has an Ethernet port, which is great. DRA821 also has a 5-port switch…
Part Number: CC2642R-Q1 Hello,
I am currently facing a challenge and I hope that you guys can support me and help me solve the problem.
I use the Honor Magic 5 pro( Cell phone ) to connect and disconnect CC2642, after multiple disconnections and connections…
Part Number: DS90UB953-Q1 Hi team,
I have asked an E2E before about how to improve the robust of the link: (1) DS90UB953-Q1: Register to improve the robustness - Interface forum - Interface - TI E2E support forums
Customer only had 9530x52[1] error about…
Part Number: UCC2813-5-Q1 I took the help of WEBENCH POWER DESIGNER for design of my Fly back converter of 56 w. My design no. 146.My user Id is info@aeshyd.com. when I click on the transformer, its showing popup with transformer information as CUSTOM…