Part Number: SN65LBC184 I'm troubleshooting a design around this part and have had 2 PCBs drawing excessive current off the 5V bus that feeds the SN65LBC184. I did not design this circuit, but 2 of these chips have failed in such a way that between the…
Part Number: SN65LBC184 Other Parts Discussed in Thread: SN65HVD72 , Hi, Team
My communication customer is using SN65LBC184 and SN65HVD72 in their smart antenna system. They want to konw the below spec of SN65LBC184 integrated TVS and SN65HVD72 integrate…
Part Number: SN65LBC184 Other Parts Discussed in Thread: SN75176A Hi,
I think the title says it all.
We are using the SN65LBC184 in our products to manage the DMX 512 protocol.
When sending informations from a light console that is using the SN75176A…
Part Number: SN75LBC184 Other Parts Discussed in Thread: SN65LBC184 What are the meanings of the SN65 and SN75 designations?
Are the parts actually identical?
Thanks.
Other Parts Discussed in Thread: SN65HVD08 , SN65LBC184 Hello,
We are considering the SN65LBC184 and the SN65HVD08 for a design, and need some help with the differences between the two with respect to the failsafe biasing during idle conditions. We notice…
Other Parts Discussed in Thread: SN65LBC184 , ISO1050 Hi all,
I use the SN65LBC184 as a RS485 transceiver in a multi-point RS485 bus configuration.
According to the data sheet, table "driver function table", the output driver should be in "Z" state if the…
Other Parts Discussed in Thread: SN65LBC184 Hi,
Our customer is looking for RS-485 device supported IEC61000-4-5.
Their surge voltage is peak-350V,1.2/50us in the condition.
I suppose that SN65LBC184 is supported IEC61000-4-5.
It is because the data sheet…
Other Parts Discussed in Thread: SN65ALS180 , SN65LBC184 , DS36277 , SN65LBC180 Is it possible to connect J1708 signals to the SN65ALS180? If so what are some of the recommended configurations and best practices?
What I would like to do is establish a J1708…
Part Number: ISO1450 Other Parts Discussed in Thread: SN65LBC184 Hi, TI Support Team
The following two parts are being used by the customer for RS-485 communication.
BCU side: ISO1450
PCS side: SN65LBC184
During the test, the following symptoms were…