Because of the Thanksgiving holiday in the U.S., TI E2E™ design support forum responses may be delayed from November 25 through December 2. Thank you for your patience.
Other Parts Discussed in Thread: SN65LVCP22 Hi,I'm FAS of Japan Disty. I have two quetions.
I downloaded datasheet & user's manual from TI's homepage. No6 and No7 Pin definitions are swapped. Which one is correct? Datasheet: sn65lvcp22.pdf …
Other Parts Discussed in Thread: SN65LVCP22 Hello, I would like to have further explanations about SN65LVCP22 2x2 LVDS CrossPoints.
The part will be used in a 2:1 mux architecture.
1. Clarification on the differences between bit rate and frequency
I have…
Using Figure 7 in the data sheet I solved for the output impedance and I got an output of 1.85pF and 86 ohms. Is this correct? Also, I'd like to know how it changes with temp/supply voltage - either in value or the graph of Fig 7.
What is the actual…
Other Parts Discussed in Thread: SN65LVCP22 , SN65LVCP15 , SN65LVCP204 , SN65LVDS250 Can the SN65LVCP22 handle switching of SGMII compliant data busses between different MACs and PHYs? This is only intended for Gigabit ethernet. This part appears to meet…
Other Parts Discussed in Thread: SN65LVCP22 We need to understand the failure mode capabilities of SN65LVCP22. There are two basic questions.
1- What failure modes does the part support?
2- Can the outputs be driven to a ground and be able to recover…
Other Parts Discussed in Thread: SN65LVCP22 Dear Sirs
I want to use two DS90UB903 and one DS90UB904.
May I use SN65LVCP22 switch between DS90UB903 and one DS90UB904?
If not, could you suggest TI's switch for FPD-Link III?
Thanks
BRS
Nat
Other Parts Discussed in Thread: SN65LVCP22
I have a customer that is using the SN65LVCP22 crosspoint switch as a 2:1 mux. There is no isolation or Xtalk specification in the datasheet. Can someone send me a test setup for isolation and Xtalk so we can…