Part Number: SN65LVDS301 Hi team,
Is there available EVM for our serializer and de-serializer (SN65LVDS301,311,302)? I can not see in the product folder.
Best regards,
Hayashi
Part Number: SN65LVDS301 Hi,
Some customers choose SN65LVDS301/302 and now want to reduce the cost, hoping to recommend a chip with similar function and cheaper.
Many thanks~
Part Number: SN65LVDS301 Dear Spacialists,
My customer is considering SN65LVDS301 and has a question.
I would be grateful if you could advise.
---
We want to use 2 of the 3 datalinks. That is, one data link is not used.
Is this usage possible…
Part Number: SN65LVDS301 Hi there,
My customer is evaluating SN65LVDS301.
They need to serialize 24bit RGB into 2ch signals so SN65LVDS301's 2ch mode seems to be good.
But they found that the PCLK of SN65LVDS301 is not enough(~30MHz), and they need…
Part Number: SN65LVDS301
dear sir:
Shàngmiàn shì wǒ cóng IC spec jiéqǔ de liǎng zhāng tú,top view wǒ lǐjiě de shì cóng chǎnpǐn top miàn kàn,top view nàgè tú biǎoshì PIN de yīnggāi shì xūxiàn ér bùshì shí xiàn? Lìngwài, wǒ xiǎng liǎojiě…
Part Number: SN65LVDS301 Hi Team,
Our customer are going to replace to SN65LVDS301 from SN65LVDS305 because SN65LVDS305 are going to be EOL.
And SN65LVDS301 has 2 more Sub LVDS channel compared with SN65LVDS305. If we replace , can we leave this…
Part Number: SN65LVDS301 I have a question.
I checked this device's product folder.
But, I could not find the ibis model for this device.
Could you give me an ibis model for SN65LVDS301?
Best regards,
ozawa
Part Number: SN65LVDS301 Other Parts Discussed in Thread: SN65LVDS93 Hi team,
my customer is evaluating the SN65LVDS301. Their issue is that the CPU has a I/O level of 3.3V, which is working without an issue, but the datasheet states that the maximum…
Other Parts Discussed in Thread: SN65LVDS301 , SN65LVDS314 , SN65LVDS302 Hi,
In the serializer SN65LVDS301 specification, there is a specification which says the maximum differential output voltage should not be more than at 200mV. My understanding…