Part Number: SN65LVDT101 Hi,
Could you please provide the SN65LVDT101 VSSOP temperature parameters as follows:
1) Maximum junction temperature
2) Junction to ambient (per footprint/PCB layers ea.)
Thanks,
Noam
Part Number: SN65LVDT101
Dears,
Our customer have some questions about SN65LVDT101. In his application, SN65LVDT101 is connected to MC100EP195 (On Semiconductor), which is a 3.3V ECL programmable delay chip. The schematic is as follows:
The 1.3V is supplied…
Part Number: DAC34SH84 Other Parts Discussed in Thread: LMK04610 , SN65LVDT101 Hi,
We are currently working on module, which holds 4 DAC34SH84s connected to one FPGA (Kintex Ultrascale). The FPGA is calculating an amplitude modulated signal with a carrier…
Other Parts Discussed in Thread: SN65LVDT101 , SN65LVDS101 Customer use SN65LVDT101 to LVDS buffer, firstly customer use 0V common voltage , and then there is big BER issue , and then they use dc couple and provide 0.18V common voltatge, it is better, just…
Other Parts Discussed in Thread: SN65LVDT101 Hello,
Usually, PECL output termination is 50ohms to Vcc-2V.
However, looking at the figure38 on page 14 of SN65LVDT101 datasheet, it is 50ohms to GND, not 3.3-2.0V.
In this case, if Vcc=3.3V, Ioh/Iol can be…
Thanks, I'll ask our FPGA designer regarding LVPECL support.
Does SN65LVDT101 has an "EP" version? Our end product will be on "LEO" mission and I was told that EP will work in that scenario.
The data sheet does not mention it but…
Part Number: SN65LVDT100 Other Parts Discussed in Thread: SN65LVELT23 , SN65LVDT101 , Hellow support team
I have two questions.
1. When restarting the SN65LVDT100, SN65LVDT101 and SN65LVELT23, how much required time from power OFF to power ON ? My customers…