Clemens, Joshua - we looked at SN65LVDT14/41 but due to cable limitations they need to run 3-wire SPI. What other SPI buffers can we suggest that meet below requirements?
"I need to run 3-wire SPI (+3.3V/GND, CS, SCK, SDI/SDO for the 4 twisted pairs). …
Part Number: SN65LVDT14 Customer tried to use the IBIS model to do the simulation. However, the results is not accetable, it looks the reflection problem is found as attached file.
Howevr, when 100 Ohm is added on the IBIS model of the SN65LVDT14's termination…
Part Number: SN65LVDT41 Other Parts Discussed in Thread: SN65LVDT14 , DRV8860 Regarding the VIH levels for the D or R inputs of the SN65LVDT14 and SN65LVDT41, can I assume that these inputs can safely tolerate 5.7V? The reason I ask is that I plan to drive…
Part Number: SN65LVDT41 Other Parts Discussed in Thread: SN65LVDT14 Hi team,
My customer is using SN65LVDT41 and SN65LVDT14 to transfer signal in two boards. And the two boards are powered in two different isolated power supply. During their test, they…
Part Number: SN65LVDT14 I plan on using the SN65LVDT14PW (20 pin TSSOP, PW package) in a space application. To properly predict the temperature, I need the junction to board thermal resistance. Can you please provide this?
Part Number: SN65LVDT41 Other Parts Discussed in Thread: SN65LVDT14 , I have tested SN65LVDT14 and the result is below.
1A
1B
1R
1.1
1.4
0
1.4
1.1
3.3
2A
2B
2R
1.1
1.4
0
1.4
1.1
3.3
3A
3B
3R
1.…
Part Number: SN65LVDT14 I have to use 1.8V power supply for differential driver and receiver on my design. Can some advise me that for SN65LVDT14 IC, is it can work under 1.8V power supply?
From the datasheet, the supply voltage range is from -0.4 ~ 4V…
If you already have pairs, then it makes sense to use differential transceivers, e.g., SN65LVDT41/SN65LVDT14. This is very helpful if the environment can be noisy.
Part Number: SN65LVDT41 Other Parts Discussed in Thread: SN65LVDT14
We plan to use SN65LVDT41 as a translator from SPT to LVDS. At this situation, 1 LVDS lane is not used.
The question is, which pin setting would be the best for non-use case? For example…