Hi Harrison,
Thank you for your patience. I have confirmed that since this package does not have an exposed pad, the parameter is referring to RθJC(top).
Regards, Amy
Part Number: SN65MLVD047A Hello,
Is it feasible to use AC coupling in customer applications? See the appendix for details。
FUXI-MLVDS Analysis-20221027.pptx
Part Number: SN65MLVD047A Hi TI,
Question1:Whether SN65MLVD047A supports hot plug?
Question2:As shown in the figure below, in this design of single point transmission and multi-point reception, damage to one point will cause damage to other devices on…
Part Number: SN65MLVD047A Other Parts Discussed in Thread: DS90LV001 Hello, is it possible to attach "normal" LVDS repeaters like the DS90LV001 to a double terminated bus driven by a bus LVDS or M-LVDS like the SN65MLVD047A?
We want to realize…
Other Parts Discussed in Thread: SN65MLVD047A , SN65MLVD047 Do we have an IBIS model available for the SN65MLVD047A?
Thanks, David
--------------------------------- David Hildebrand Analog Field Applications South Region Texas Instruments, Inc. Office: 214-479…
Other Parts Discussed in Thread: SN65MLVD047 What's the difference between these two parts? Everything looks identical. Only slight differences I could find were small variations in the finish (gold/copper) ppm's in the environmental information, but…
Other Parts Discussed in Thread: SN65MLVD047A I'm designing MLVDS interface.
Want to use sn65mlvd047a driver.
Using multi-drop -- 1 driver 8 receivers.
The '047a spec requires 55 ohm max load resistance.
The TI paper slla038b says multi-drop only…
Part Number: SN65LVDS1 Other Parts Discussed in Thread: SN65MLVD047A , Hello,
I need to drive 6 LVDS recievers with only one driver in a multidrop topology, at 100MHz clock frequency.
I didn't find a single MLVDS driver ( there is 2 or 3 components with…