I am planning to use the SN65MLVD202A in full duplex mode. I see that the input capacitance is 5pF on each input and 3pF across the inputs. Please see the attached schematic. Is this what the dummy load should look like?
All pins need to operate within the absolute maximum ratings in the datasheet. 5V is too high and even greater than the supply voltage. It will put device into undetermined state and possible damage the device. Can customer replace it with SN65MLVD202A…