Part Number: SN65MLVD206B Hi team
My customer is using SN65MLVS206B to design M-LVDS backplane bus, and need to test the max signal rate.
Is there an Eye Mask for M-LVDS in BU side for transceiver waveform test?what is the method in BU side to test…
Part Number: SN65MLVD206B Other Parts Discussed in Thread: SN65MLVD204B , SN65MLVD204A , Hello support team,
I have known that ESD rating (IEC 61000-4-2 Contact charge ± 8 kV) and noise immunity of SN65MLVD204B are higher than SN65MLVD204A. e2e.ti.com…
Part Number: SN65MLVD204A Other Parts Discussed in Thread: SN65MLVD206B Hi team,
If the data rate is 5Mbps, is there any risk if SN65MLVD204AD pair with SN65MLVD206B? Thanks.
Part Number: SN65MLVD206B Hello,
I would like you to confirm cable requirement for M-LVDS.
Here is configuration for SN65MLVD206B (4 Transeiver is used).
Could you please confirm cable requirement for above configuration ?
Best Regards,
Part Number: SN65MLVD206B Hi Team
My customer is looking for SN65MLVD205B/207B, but I can not find the order information, could you help to confirm the RTM date of 205B and 207B? thanks.
Hello,
As a start please check that your design and layout follow the recommendations in the datasheet. Please pay special attention to bypass capacitance (section 9.2.3.2). Another thing to do is to try to reduce the spikes on the input signal to…
Other Parts Discussed in Thread: SN65MLVD206B I am looking for interface IC that can be used for MIL-STD1553B Transceiver
For example :
SN65MLVD203BRUMR
Thank you
Regards
Ramin Tavassoli
Hi Lee-san,
Thanks for your prompt response on this.
I'm a little bit confused, so Could you tell me the definition of the Hysteresis?
SN65MLVD206B has the hysteresis but I didn't understand well the difference between SN65MLVD206B and DS91M040…
Hi Jonathan,
For the differential use case, >200 Mbps is generally too high for a higher-voltage interface like RS-422. Have you considered using a different signaling standard like LVDS or M-LVDS for this? For example, the SN65MLVD206B transceiver…