Part Number: SN74ABT541B When simulating IBIS model for SN74ABT541B, output was not normally the condition of over than 3.5Vout.
(SN74ABT541B Vcc: 4.5V ~ 5.5V)
Is there IBIS model for SN74ABT541B with 5V output condition?
By the way, simulation condition…
Part Number: SN74ABT541B
Hello Team,
SN74ABT541B IO (Current into any output in the low state) max is 128mA as shown in ds page 3.
May I know if there is a total current maximum spec for the 8-ch buffer? The total current flows through VCC or ground…
Part Number: SN74ABT541B Hi,
is there a value for the internal output pull-up resistance given? Alternatively a graph for the Output-Voltage over Output-current.
I found the paper "designing with logic" from TI, there is output resistance Ro for the SN74ABT240…
Part Number: SN74ABT541B Hello guys,
One of our customers is evaluating SN74ABT541B. When they checked output (Y1) of the device on their PCB, a overshoot of output (Y1) as the attached data. Input signal (A1, ch2_skyblue), Output signal (Y1, ch1_blue…
Part Number: SN74ABT541B The data sheet for this device only lists maximum operating ambient temperature. What is the maximum operating junction temperature?
Part Number: SN74HCS244-Q1 Other Parts Discussed in Thread: TMUX1308 , , SN74LVC125A , SN74LVC3G17 , SN74ABT541B-Q1 Hi:
I'd like to design 8 channels demultiplexer for JTAG (Jtag repeater).
Front-end use 4*TMUX1308 as demultiplexer.
(TDI, TDO, TCK, TMS…
Hello Wade,
Yes, the question for the total max current spec is for SN54ABT541 ( 8-ch logic).
But Emyrs also help comment SN74ABT541B max current spec which should be the same with SN54ABT541 due to the latch up 500mA spec for both parts.
Below is the…