Part Number: SN74AHC08Q-Q1 Hi, Team,
When connecting two logic ICs(a IC's OUTPUT and another IC's INPUT), are there any precautions for connecting both directly? Because; Now A customer is considering a circuit configuration that connects the output…
What if Vin is above Vcc? as explained take example: Vcc=5V and Vin is 6V.
Will this work, or does any current limiting resistor has to be added to the input?
I refer to datasheet page 2, note 1:
https://www.ti.com/lit/ds/symlink/sn74ahc08q-q1…
The difference between the SN74LVC08-Q1 and the SN74LVC08A-Q1 is that only the latter exists.
If you meant the SN74ALVC08-Q1: its inputs are not 5 V tolerant.
The HC is slower and has lower drive stength than the (A)LVC. If the HC works in your…