Part Number: SN74AHC1G04 Other Parts Discussed in Thread: SN74LVC1G57 , SN74LVC1G14 hi dear supporting team,
customer found PIN2 of SN74AHC1G04QDCKRQ1 has a short term -0.8V voltage, while in the d/s, it mentioned the min voltage is -0.5V, the waveform…
Part Number: SN74AHC1G04 Hi all Would you mind if we ask SN74AHC1G04? <Question1> 1Pin(NC) does not connect to any pin internally, right? <Question2> Which is the better handling for NC pin? -Connection to GND(Does it help radiation of heat?) -Connection…
Hi Matt,
To answer some of your questions:
We don't model the input clamp in this part's spice model.
Based on the datasheet section "6.1 Absolute Maximum Ratings":
Vi, Input Voltage Range is recommended not to exceed -0.5V on the low side and…
Part Number: SN74AHC1G04 Hello, I have a request about SN74AHC1G04.
I want the data of VOH and VOL.
Conditions VCC=5V IOH=-1mA IOL=1mA
Could you give me the data as follows, please?
Regards, Dice-K
Part Number: SN74AHC1G04 Dear Technical Support Team,
Could you share the VIH(min) and VOH(min) with 3.3V Vcc?
The datahsheet of SN74AHC1G04 show just 3V Vcc condition, but I use 3.3V.
Best Regards,
ttd
Part Number: SN74AHC1G04 Hello, I have a request about SN74AHC1G04.
Is there the following data? ・The variability of output resistance. For example, 70Ω(High) 45Ω(Low) @25℃ or ・Vo (output voltage) vs Io (output current) High and Low
[supplementary…
Other Parts Discussed in Thread: SN74AHC1G04-Q1 , SN74HCU04 , SN74AHC1GU04 Hi Team,
My customer considers to use SN74AHC1G04-Q1 for crystal oscillation circuit and I was asked the following. Is this device single stage inverter? Datasheet(logic diagram…
Hi
I have one simple question.
Is it possible to input any 5V signal to input pin if it is no supply voltage?
I would like to make sure there is a possibility that such a situation occurs on the customer's board.
Regards,
Koji Hamamoto
Other Parts Discussed in Thread: SN74AHC1G04 I'd like to use the buffer by translator converting small signal level to LVTTL.
I'm wondering which is the maximum frequency properly available with the SN74AHC1G04.
or how can i find out the available…
Part Number: ADS8548 Other Parts Discussed in Thread: SN74AHC1G04 Tool/software: I have a question about ADS8548.
I produce some ads8548 boards. The refio pin of some boards is 4.966V, and some are normal(2.5V). why?