Part Number: SN74AHC541 Other Parts Discussed in Thread: SN74LXC8T245-Q1 , SN74AHCT244Q Hi,
In our project we are using this buffer SN74AHC541QPWRG4Q1.In my microcontroller working on 3.3V and motor driver IC 5V.
I have to control the speed of the motor…
Hi Clemens, Ok. I will need to do some measurements. You are right: in this instance I don't actually need a transceiver. The SN74AHC541 is a good suggestion, only problem is we are space constrained so it's package offerings are far too big. Thanks…
Part Number: SN74AHC541 Hi All,
I have a question about SN74AHC541.
Please tell me the values of VIL max and VIH min when VCC = 5V.
Best Regards, Ishiwata
The TXB does not support these supply voltages; VCCA must not be larger than VCCB.
The high level of TTL signals is 3.3 V. Are you using TTL signals or 5 V signals?
The TXB is designed for auto-bidirectional applications, which results in many restrictions;…
Part Number: SN74AHC541 Hi Team, I understand storage temperature of SN74AHC541 is -65~150 C as the following. Is there Absolute Maximum ratings of Tj (junction temperature)? Best Regards, Yaita
LVDS repeaters are designed for LVDS signals.
There are clock buffers like the LMK1C1104/LMK1C1108. But you could also use plain logic buffers like the SN74LVC125A/SN74LVC541A/SN74AHC125/SN74AHC541/SN74LV125A/SN74LV541A.
Part Number: SN74AHC541-Q1 Hi team,
My customer asks question about VIH and VIL for OE2 of SN74AHC541-Q1.
There is a Table of “recommended operating conditions” in the datasheet, is it also applicable for OE2 port?
If not please provide…
Part Number: SN74HCS151 Other Parts Discussed in Thread: SN74CB3Q3251 , SN74AHC541 , SN74AHC1G125 Hi Team,
As title, do we have solution can achieve below requirement?
Roy
2× SN74LVC157A, or SN74AHC157 with lower drive strength.
You could also use a single buffered or analog multiplexer (SN74LVC1G97 or SN74LVC1G3157) to drive eight buffers (SN74LVC541A or SN74AHC541).