Part Number: SN74ALVC244 Hi team,
What's the difference between SN74LVC244 A PWR and SN74 A LVC244PWR
how to choose the best one on the server application?
Part Number: SN74ALVC244 Other Parts Discussed in Thread: SN74ALVTH162827 , SN74LVTZ244 I had a question about SN74ALVC244. Does it have diode to GND or VCC on the pins? In a hot swap application, ( Most of logic IC s has internal diodes at supply and…
Part Number: SN74ALVC244 Other Parts Discussed in Thread: SN74AVC24T245 , SN74AVC16834 Team,
my customer is looking for a 16bit buffer similar to 74ALVC244, but in a package that is smaller than 50mm^2, eg a BGA package. They need 0.8mm pitch.
Best…
Part Number: SN74ALVC244 Other Parts Discussed in Thread: SN74LVT244B , SN74LVC244A Hi
From the datasheet, the output of SN74ALVC244 is limited by VCC.
Is this relative with the internal ESD diode?
Do we have similar buffer but no such limitation…
Part Number: SN74ALVC244 Dear PIC,
Our customer ask us the figure about VIH and VIL when the power supply voltage is 2.25V.
they tried to refer the datasheet, but there are not described in it. Could you kindly tell us them?
Best Regard,
Part Number: SN74ALVC244 Hi Team,
We've received an inquiry from a customer about two SN74ALVC244 with same supply voltage level (3.3V) but different power source. The output of the first buffer (A) goes to another buffer (B) and there is a 1k ohm pullup…
Part Number: SN74ALVC244 Kindly provide us the Tape Pitch, Tape Width and Pin-1 Orientation for below MPN:SN74ALVC244PWR
This information is not available on provided datasheet: www.ti.com/.../sn74alvc244.pdf
Hi,
I agree with Clemen's response on this. Using a unidirectional device will simplify your design work as there are less things to worry about. This is because as Clemens mentioned, if there are any large reflections on the transmission line then…
Part Number: SN74ALVC244 Hello,
I wish to connect the Vcc to 1.8V and connect the the outputs/inputs pins to 3.3V signals, Is the part is 3.3V−Tolerant?
Best regards,
Emanuel