Part Number: SN74ALVTH16245 Hi,
Is SN74ALVTH16245 an electrostatic sensitive device?
If it is electrostatic sensitive device, HBM (human body model), CDM (charging device model), MM (and its model), IEC61000-4-2 are how many? I did not find relevant information…
Part Number: SN74ALVTH16245 Hi team.
I'd like to know how much signal frequency can it input.
Can I refer to ''Input transition rise or fall rate'' in the data sheet?
∆t/∆v = 10ns/V
Input = 5V
10(ns/V) / 5(V) = 2(ns)
F(Hz) = 1 / …
Part Number: SN74ALVTH16245 This is Joong-hyeok Lee, DMSMS researcher of Leoinnovision. Leoinnovision is the official EOL(End Of-Life)/obsolescence part manager of Korean Military (Army, Navy, Air force) and PLM agency of many defense industries (Hanwha…
Part Number: SN74ALVTH16245
Hi Team, Could you tell me the value of Theta JC (Junction to Case) for the following? ・SN74ALVTH16245GR ・CDCV304PW ・SN74LVC2T45DCU ・SN74LVC541APW I would also like to ask Tj-max for these. Best Regards, Yaita