Part Number: SN74AUC08
Hi Team,
Looking for a low latency device to isolate clock signals from a CPU board to a Line Card. (dip switch like device that can isolate the incoming clocks while the line card is not turned on)
Does the SN74AUC08 handle…
Part Number: SN74AUC08 Hi Sirs,
Sorry to bother you.
We would like check SN74AUC08RGYR
B
ψJ-T(C/W , thermal resistance)=? and Tj Max.( C, Junction Temp.) =?
C
θJ-C(C/W , thermal resistance)=?
Could you help…
Part Number: SN74AUC34 Other Parts Discussed in Thread: SN74AUC04 , SN74AUC08 , SN74AXC1T45 , SN74AUC2G240 , LMK1C1103 , SN74LVC257A-Q1 , SN74ALVC04 Tool/software: Hi,
My design uses a mix of LVCMOS components. I have chosen these components for a reason…
Part Number: SN74ALVC08 Other Parts Discussed in Thread: SN74AUC08 Tool/software: Hi,
I am using this quadruple, 2 input AND gate in a clock tree. The input will see an LVCMOS 1.8V Clk @ 30MHz, 15MHz, 1M, 2M and 500k. I am debating if cross-talk will…
Hi Amtech, The SN74AUC08 is a quad AND gate with the propagation delay you want, but it is not pin to pin with the CD4081B. It also is not compatible with 15-V logic.
The CD4000 family is the only family we have that supports 15 V. Why are you looking…
Hello Maxime,
In the datasheet, it states that:
The ’HC4046A and ’HCT4046A are high-speed silicon-gate CMOS devices that are pin compatible with the CD4046B of the “4000B” series.
This indicates that the pinout of these devices are very similar…
AUC will be the fastest logic. The rise time will depend on the load and VCC. With a light load 5pf or so the rise and fall times should be around 1/2 ns.
Its max Vcc is 2.7V.
SN74AUC1G32 SN74AUC32
SN74AUC1G08 SN74AUC08