Part Number: SN74AVC16827 Other Parts Discussed in Thread: SN74AUC244 Hi,
Could you please tell me the 100MHz and 200MHz operating conditions for SN74AVC16827 ? * e.g.: VCC, CL(output load capacitance, etc)
Best regards, Kato
Hi,
Thank you for the response.
SN74AUC244 doesn't sit on existing footprint, I already have my board with me. SN74LVC244ADWR was SOIC package and SN74AUC244 is QFN.
Please suggest an IC of same pin out and same package + footprint that has 8mA…
Part Number: SN74AUC07 Other Parts Discussed in Thread: SN74AUC244 , SN74LVC244A , SN74AUC245 Dear experts,
Customer is looking for re-driver to connect SD card 6 pins (Data0~3, CMD,CLK).
Currently, they have problem with High speed(200MHz) communication…
Chris,
Thanks for the reply. Anything faster that the SN74LVC244 in the ZQN package? My customer is space constrained.
Or any plans to add the SN74AUC244 into a smaller package?
- Aaron
The resistor will not be needed on the 3.3V side.
You could also just use a buffer that is overvoltage tolerant on the inputs. SN74AUC244 you cuold set VCC at 1.5V and the input could be 3.3V. The part would translate down to VCC and also have buffering…
Part Number: SN74AXC8T245-Q1 Hi team,
I have one question about SN74AXC8T245-Q1. We plan to use this device for 1V8 to 1V8, the purpose is to pull high /OE pin to disconnect the RGMII(125Mhz) signal before the whole system bring up.
My question:
1. Can…