Part Number: SN74AUP1G07 Other Parts Discussed in Thread: SN74LVC1G07 , SN74LVC1G125 , SN74LVC1G126 Hi I am trying to understand the what is meant when some data sheets indicate support for Ioff some data sheets like the subject part indicate Ioff Supports…
Part Number: SN74AUP1G07 Hi,
I have a question about the absolute maximum rating of Io listed in the data sheet P.4. In "Continuous output current", the max value is specified as ±20mA. In "Continuous current through VCC or GND", the max…
Other Parts Discussed in Thread: SN74AUP1G07 Hi Team,
I'd like to know internal block diagram of SN74AUP1G07. Can you share this or explain operation thing?
Also, in D/S P11, what is meaning of "Bus Contention" ?
for this reason, When the…
Other Parts Discussed in Thread: SN74AUP1G07 Can you tell me the behavior of the SN74AUP1G07 when VCC is grounded and power is applied to Y pin? Is there a diode between these pins (Anode on Y and Cathode on VCC)?
I ask because of this specification isn…
The LVC family (from any manufacturer) is designed for 1.8 V … 5 V.
The only device covering 1.1 V … 3.3 V is the SN74AUP1G07. The SN74AUC1G07 does not work above 2.5 V, but has higher drive strength.
Other Parts Discussed in Thread: SN74AUP1G07 the SN74AUP1G07 is a single buffer with open drain outputs. As the figure 5 of datasheet, is there any Vpu limit in the design?
Other Parts Discussed in Thread: SN74AUP1G07 , SN74AUP1G34 I am using 2 SN74AUP1G07 O/D buffers connecter to each other for doing some voltage translation. I want to confirm the amount of current needed to source the input of this chip to a high state and…
Other Parts Discussed in Thread: SN74AUP1G07 , TS5A3159 Hello,
Our customer would like to use one buffer IC for both signals of HPD and CBUS.
Then, I think that SN74AUP1G07 may be used as buffer IC of these signals by one device.
Can SN74AUP1G07 as buffer…