Part Number: SN74AUP2G07 Tool/software: We are proceeding with the certification for the product containing the IC SN74AUP2G07DSFR.
If EMI/EMC and Safety tests have been conducted on the unit or any other tests have been conducted on the unit, please…
Part Number: SN74AUP2G07 Other Parts Discussed in Thread: SN74AUP2G08 Hello, we found different stencil designs(opening and thickness) recommended on data sheets of SN74AUP2G07(6-pin SON, 0.35mm pitch) and SN74AUP2G07(8-pin SON, 0.35pitch), see images…
Part Number: SN74AUP2G07 I would like to order SN74AUP2G07DCKR 3Kpcs. But It it impossible to order due to below reason.
Please advise what is the meaning in details and advise other method to buying.
Product SN74AUP2G07DCKR cannot be supported from available…
Part Number: SN74AUP2G07 Other Parts Discussed in Thread: SN74AUP1G07 , SN74AUP3G07 , SN74AXC2T45 hi,
i am using SN74AUP2G07 with 1.5V VCC and directly connect the OD output to input pin of other 3V device. the OD output was pull up to 3V through 10K. …
Part Number: SN74AUP2G07 Other Parts Discussed in Thread: SN74AXC4T245 , SN74AXC2T45 Hello experts,
My customer is looking for buffer IC;
Requirement : single end signal, 1.25V -> 3.3V, 20Mbps, 2~4ch.
They plan to operate with Vcc=1.5V.
But SN74AUP2G07…
Part Number: SN74AUP2G07 Other Parts Discussed in Thread: SN74LVC2G07 Hi TI team
SN74AUP2G07 can be used in applications such as UART?
Could you review my schematic?
Is it okay?
Please refer to the app note:
I think the curves shown here looks good to me as they are < 10ns/V.
The SN74AUP2G07 as suggested may be another option for 3.3V usage but I wont be suggested with a 5V pullup.
I guess you want open-drain outputs? Use the SN74LVC2G07. (The SN74AUP2G07 has a lower drive strength.)
The smallest buffer with at least four outputs would be the SN74LVC07A, which actually has six; you might want to use 2× SN74LVC2G07 instead.…
From the description, I'm not certain if the signal is being translated down from 3.3V to 1.8V or up from 1.8V to 3.3V.
You can do either with an open-drain buffer such as SN74LVC2G07 or SN74AUP2G07.
You can also use a buffer/translator like SN74LV1T34…
Other Parts Discussed in Thread: SN74AUP2G07 Hello SLL Friends!
I was looking at the SN74AUP2G07 datasheet, and I noticed that is it has VOH and IOH in the electrical specifications section. The AUP2G07 is an open-drain device, and I haven't seen VOH and…