Part Number: SN74AUP3G34 Tool/software: Hi Team,
What is the maximum frequency of signals SN74AUP3G34DQER could support without any signal integrity issues
We have planned to use in a system which works max 30MHz
Awaiting for your reply…
Part Number: SN74AUP3G34 Other Parts Discussed in Thread: SN74AUP1G34 Can I get IBIS model for the SN74AUP3G34 part? I only see spice model for the part.
Ibis model for different part with similar CMOS driver / receiver also works.
Part Number: SN74AUP3G34 Other Parts Discussed in Thread: SN74LVC126A Tool/software: Hi team,
My customer has been looking for the non inverting buffer which meets the spec below. non inverting buffer is used for the buffer of SPI(MOSI, MISO, SCLK)…
Part Number: SN74AUP3G34SN74AUP3G34DC - Please let me know whether the stated part number is with push pull configuration output? If so i can Pull_Up and Pull-Down output signals ?
Other Parts Discussed in Thread: SN74AUP3G34SN74AUP3G34 - who owns the Marketing and pricing for this part? working a 100k quote at Cisco. thanks.
bill
Part Number: TXU0104 Other Parts Discussed in Thread: SN74AVC4T245 , SN74LV1T08 , SN74LV4T125 , SN74AUP1T17 , SN74AUP1G34 , SN74AUP3G34 HI team,
Can you please support to select right parts to satisfy below requirements?
Vcc_input = 1.8V
Input:…
Part Number: SN74AUP3G07 Other Parts Discussed in Thread: SN74AUP3G34 , SN74AUP3G17 Hi Expert,
Customer need a I2S buffer to support Audio serial data interface bus output(SDOUT,BCLK,FSYNC), and BCLK need to support 25MHz , do you have recommend solution…
Hi Irfan,
Based on this schematic, I'm concerned because I do not see any pull-up resistors on the output. SN74LVC2G07 is an open-drain output device, so it needs to have a pull-up resistor to 1.8V if you want to high-level output to be 1.8V. [FAQ]…
Part Number: SN74AUP2G34 Other Parts Discussed in Thread: SN74AUP3G34 , , SN74AUC16245 Hi Sir
Reference design use 74AUP2G34 to do 14bit parallel digital video buffer
We will like to check 4bit or 8bit solution ,if have 16bit solution it will be…