Part Number: SN74AVC1T45 Hi,
I want to understand if this chip can handle a frequency of 40MHz LVCMOS clock on its input?
The datarate says 500MBPS so i am assuming the frequency it can handle is nearly 500MHz for 1.8V to 3.3V.
Is this correct? the datasheet…
Part Number: SN74AVC1T45 Hi Team,
Would you advise the concern of usage if exist in below case and if it will be a failure mode, could you advise me
the what failure mode is concern?
According to datasheet, there is "This single-bit noninverting bus transceiver…
Part Number: SN74AVC1T45 Dear SIR:
Good day!! May I have some question regarding "SN74AVC1T45".
If SN74AVC1T45 pin 6 we have connect to 3.3V Power
pin 5 we NC.
pin 2 we have connect to GND
pin 4 we have…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: 74AVC1T45 , SN74AUC1G125 Hi,
need voltage translator for 25MHz clock - 3.3V to 1.8V.
can i use the 74AVC1T45 ? what is the advantage of 74AXC1T45?
Erez
Part Number: SN74AVCH1T45 Other Parts Discussed in Thread: SN74AVC1T45 Hello,
I don't want to scan the datasheets side by side. The only difference I could find so far is related to the level shifting (as stated in the document header). But both documents…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 Hello Support team,
Are there specification or data of the phase noise of SN74AVC1T45? Is it possible to achieve -135dBc/Hz@100kHz, -140dBc/Hz@1MHz with SN74AVC1T45?
Best Regards, Hirokazu…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74AXC1T45 , SN74LVC1T45 , Hi,
My customer is considering voltage translator for 3.3V to 1.8V with direction control. I think both are applicable, but I want to know if there's any other difference…
Part Number: SN74AVC1T45 Other Parts Discussed in Thread: SN74LVC1G07 , SN74AUC1G125 Hi Team,
May I know what's difference between these devices? pull-low voltage level, separated 2 Vcc rails, and ...
SN74AVC1T45
SN74LVC1G07
SN74AUC1G125