Part Number: SN74AVC2T245 Hi, I'm currently using SN74AVC2T245 with VCCA = 1.8V and VCCB support voltage like 1.2V, 1.5V, 1.8V, 2.5V, 3.3V. I have attached the schematic as below:
When I drive signal from port A to port B, I noticed that the different…
Part Number: SN74AVC2T245 Hi sir,
My customer got SN74AVC2T245RSWR and SN74AVC4T774PWR IBIS model for simulation purpose.
Should they need to add input and output capacitance in simulation?
Thank you.
Regards,
Allen
Part Number: SN74AVC2T245 Other Parts Discussed in Thread: SN74AXC2T245 , SN74AVC2T244 Hi Sir,
We encountered a weird issue on customer factory they reported they designed SN74AVC2T245 for Dmic level shift 1.8v (PCH) to 3.3v (Dmic module).
But some of…
Part Number: SN74AVC2T245 Other Parts Discussed in Thread: SN74AXC4T245 , SN74AXC2T45
Hi,
I have a question regarding the SN74AVC4T245RGYR and SN74AVC2T245RSWR:
Is there a power-up sequence for the components? if only one supply is ON and the other is…
Part Number: SN74AVC2T245 Team,
This part is used on the
UART Tx and Rx lines between two boards, called B1 and B2. We have a scenario where, on power up
the Tx messages from B1 are not being received on B2.
The board with the SN74AVC2T245 does not…
Part Number: SN74AVC2T245 Hi Sir,
As the title, customer would like to re-confirm the status of SN74AVC2T245 during the power down.
If system be power down does control pin (DIR, OE) and data pin (A/B port) become Hi-Z?
BTW, their OE connect to GND directly…
Part Number: SN74AVC2T245 Other Parts Discussed in Thread: SN74AXC2T245 Hi Sir,
As the title, customer got some case that they would like to use our SN74AVC2T245 for the Dmic data & clock level shift.
But they got the case, they might have different…
Part Number: SN74AVC2T245 Hi,
There is no IO available to control the OE pin of SN74AVC2T245. So i am wondering if it is OK to connect OE pin to ground directly. Is there any risk? A port is 1.8V and B port is 3.3V.
Regards,
Yangbo
Part Number: SN74AVC2T245 Other Parts Discussed in Thread: SN74AVC2T45 Hi,
May I know what are the differences between SN74AVC2T245 and SN74AVC2T45?
Thanks,
Philip