Part Number: SN74AVC2T245-Q1 Hello I am Juan Jacinto Montenegro, from Rother.
We are designing a PCB, for which we will be using the SN74AVC2T245-Q1.
In our specific case, the signals from this component would be connected as follows:
VCCA (3…
Part Number: SN74AVC2T245 Tool/software: Hi TI,
About the SN74AVC2T245 Hspice model.
The VCC & data pin definition in the Hspice model was not found in the Datasheet(Fig.1).
Q1. How to connect VCC and data pin?
In my topology(Fig.2), the a1 and…
Hi Liang,
Liang Barry said: SN74AVC2T45-Q1
You may use SN74AVC2T245 IBIS Model or any other IBIS model from the AVC family.
Liang Barry said: TXV0106-Q1
Please note that although the device is planned to be released to market soon, it is…
Part Number: SN74AVC2T245 Other Parts Discussed in Thread: TXS0102 Hi,
Q1. Do the SN74AVC2T245 is suitable for Open Drain signal level shifting?
Please refer to the attached image..
Q2. I am looking to shift 3.3V open Drain signal to 1.8V logic…
Hi,
Thanks for the quick reply. Which TI part do you suggest?
I have shortlisted these 2 in the order of preference. Am I choosing the right one?
SN74LVC2T45-Q1
SN74AVC2T245
Thanks in advance.
-Shashi.
Other Parts Discussed in Thread: SN74AVC2T245 , SN74AVC4T245 , SN74LVC2T45 Hi Team,
Our customer requests us the information of the thermal characteristic of SN74LVC2T45YXPR. Could you provide us the following two information ?
[Q1] What is Theta…
Hello Sreenivasa san
Thank you for your reply.
> Can you please provide some additional details on how the data is being sent and received.
Can you check if all the basic hardware diagnostics tests on the board…
Dear J,
I’m connecting the PHY to the XCZ7020 SOM using RGMII. When I attach my laptop to the RJ45, the link LEDs blink, but I cannot ping the board.
I’ve also observed a separate — but probably related — problem with the strap-addressing: I hard…
Hi,
Attach the Ultra96 V1 schematic. Our board produced the same. And the current of each power rail cannot be measured. Each Buck did not connect parts such as the INA226, and even if I measure it in another way, I think the measurement values are…