Other Parts Discussed in Thread: SN74AVC32T245 Hello, Our customer is evaluating SN74AVC32T245. I got the questions from them.
1. Could you please let me know the allowable time between power supply to VCCA(or B) and power supply to VCCB(or A) ?
2. If power…
Part Number: SN74AVC32T245 Hi,
I want to level shift the 1.8V signals from the controller to 2.5V for DPHY. This requires high data rates.
So, What is the max. data rate supported while translating 1.8V signals to 2.5V using SN74AVC32T245?
Regards,
Shanu…
Part Number: SN74AVC32T245 Hi,
We are using SN74AVC32T245 for voltage level translation of clock and its associated data port signals from 1.8V (A-side) to 3.3V (B-side). The data bus is 24-bit width and the maximum clock frequency is 150MHz.
What will…
Part Number: TFP410 Other Parts Discussed in Thread: SN74AVC32T245 Hi, In our project, we are interfacing TFP410 with Xilinx FPGA . The IO bank voltage of FPGA will support up to 1.8V only. We need to map Data signals to FPGA, we are using SN74AVC32T245…
Other Parts Discussed in Thread: SN74AVC32T245 Hi,
Does SN74AVC32T245 work at the 150MHz as the clock frequency normally when transrating the 3.3V cmos logic signal to the 1.8V cmos logic signal ?
We understood that it is difficult to work at 150MHz as…
Other Parts Discussed in Thread: TXB0304 , TXB0108 Hello,
Does this part allow by-direction translation at the same time?
E.g. side A is 3.3V and side B is 1.8V. Can side A send data to B and also receive data from B, either from different pins at the same…
Other Parts Discussed in Thread: SN74AVC32T245 , TXB0108 Hello,
My customer uses the SN74AVC32T245, try to change DIR during operation.
He checked switching characteristics about DIR on the datasheet.
But there is not mentioned that.
How about delay time…