Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 Hi
Can I use SN74AVCH8T245 for SPI lines voltage level translator (1.2V to 1.8V)?? Since datasheet says it is designed for asynchronous communication between data buses.. So please…
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74AVC8T245 , Hi e2e,
I am looking for a 3.3V to 2.5V level shifter. It’s not necessarily bi-directional. Down-conversion from 3.3 to 2.5V is good enough.
Clock is 125MHz and data rate…
Part Number: SN74AVCH8T245 Hello to the team ,
Data-sheet of SN74AVCH8T245 recommends to avoid using pull-up/pull-down resistors for the inputs of the component.
However, the SCLA015 document (Application Report on bus-hold circuit) says the opposite: "Another…
Part Number: SN74AVCH8T245 Other Parts Discussed in Thread: SN74LVC07A , SN74LVC06A
Hi,
I use SN74AVCH8T245PWR level shifter for driving LEDs. Presently I use this for for enabling the LEDs with 1.8V IO. The GPIO_LED signals are driven by processor.
Page…
Part Number: SN74AVCH8T245 My customer is looking to use the SN74AVCH8T245 with a display controller. The display controller has a VIL of 0.2xVDD, at 3.3V this is 0.66V. The SN74AVCH8T245, has a specified max VOL of 0.7V @ 3V and Io = 12mA. Would this…
Other Parts Discussed in Thread: SN74AVCH16T245 , SN74AVCH8T245 Hi,
I have some unused inputs on both sn74avch16t245 and sn74avch8t245. can I connect them to ground? will it cause unwanted current drawn?
It is mentioned in the sn74avch16t245 datasheet that…
Part Number: SN74AVCH2T45 Other Parts Discussed in Thread: SN74AVCH8T245 Hi,
Good Day.
Customer had a question regarding SN74AVCH2T245 and SN74AVCH8T245. He connect either input pins or output pins or one of these two ICs to a circuit board node which…
Other Parts Discussed in Thread: SN74AVCH8T245 Hi,
I calculated ICCB maximum for SN74AVCH8T245RHLR voltage level translator as per the following equation:
ICCB = static ICCB + dynamic ICCB
as per the following link
The maximum ICCB current as per my calculation…
Part Number: SN74AXCH8T245 Other Parts Discussed in Thread: SN74AXC8T245 , , SN74AVCH8T245 Dear Sir:
The current system uses SN74AXC8T245 as the I2S&SPDIF buffer.
Because SN74AXC8T245 is out of stock recently, can I use SN74AXCH8T245 instead?
Best…