Part Number: SN74AXC4T245 Dear team
There is a good news that we design in SN74AXC4T245BQBR in customer's new project.
Could you help to review the schematic?
Many thanks
Denny
Hello,
I want to use SN74AXC4T245BQBR part as voltage level shifter (for SPI Application) in my Project. From the datasheet I have learn that VCCA and VCCB both can supply on any voltage range from 0.6V to 3.3v. When I refer a reference design in that VCCA…
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: SN74AVC4T245 Hi there,
Currently I'm studying multiple pairs of 3.3V to 1.8V UART level shift option for my design, so far my plan is use SN74AXC4T245 for each two pairs of UART, and take SN74AVC4T245…
Part Number: SN74AXC4T245 Hi,
We have one question.
Could you please let us know the Min VOH voltage on VCCA=VCCB=3.3V?
We can find Min VOH on another conditions, such as VCCA=VCCB=3.0V and below. But we want to know them on VCCA=VCCB=3.3V. Please advise…
Part Number: SN74AXC4T245-Q1 Hi team,
Here is a question from my customer, SNAXC4T245 is used in an automotive gateway module. The output skew is a key spec. But I can't find this in datasheet. Do you have the result of Max skew between 4 output channels…
Part Number: SN74AXC4T245 Hi Expert,
The engineer would like to run the SN74AXC4T245PWR to 312.5MHz Clock applicant for voltage transfer.
Pls advice whether SN74AXC4T245 can support this or not.
If not,pls guide us the suitable solution for this case.T…
Part Number: SN74AVC4T245 Other Parts Discussed in Thread: SN74AXC4T245 Hi Team,
We would like to ask your help regarding the customer's inquiry below.
If i am using SN74AXC4T245 in my design instead of SN74AVC4T245DGVR as in the image, when ever i…
Part Number: SN74AXC4T245 The SN74AXC4T245 data sheet states on page 1, 2 nd para in column 2, that the xOE# pins must be pulled to Vcca to ensure IOs are high-impedance during power up/down.
In section 9.2, there is a note that the xOE# pins may be pulled…