Part Number: SN74AXC4T245-Q1 Hi team,
Here is a question from my customer, SNAXC4T245 is used in an automotive gateway module. The output skew is a key spec. But I can't find this in datasheet. Do you have the result of Max skew between 4 output channels…
Part Number: SN74AXC4T245-Q1 Hi team,
I want to check if the pull up/down resistor can be placed at input I/O port of SN74AXC4T245-Q1 (1.8V to 3.3V). This is because a slave deivce has a shared port (Mute/Address pin). At the power up sequence of the slave…
Part Number: SN74AXC4T245-Q1 Hello, Is it possible to request for the slew rate at the following conditions? VCCA 1.2V to VCCB 2.5V trasition at 200Mbps driving a load <15pF. Thank you
Hi, Clemens
I have fuel questions need check as below.
1. Is SN74AXC4T774-Q1 and SN74AXC4T245-Q1 design different between those? a. SN74AXC4T774-Q1 is design for more direction-control flexible? b. SN74AXC4T245-Q1 is design for more output enable flexible…
Part Number: SN74AXC4T245 Other Parts Discussed in Thread: TXV0108-Q1 , TXV0106-Q1 Hi Team,
We are using the SN74AXC4T245PWR IC for level translation. In the datasheet, it is given that the data rate supported whea.n translating from 1.8V to 3.3V is up…
Part Number: SN74AVCH4T245 Other Parts Discussed in Thread: SN74AXC4T245-Q1 , SN74AXCH4T245 Dear Team,
We are using 74AVCH4T245BQ-Q100 in our design and we need FFF alternate for this chip.
Can you please suggest best alternative in terms of direct replacement…
Hi Dylan
Thanks.
What is the difference between SN74AXC4T245 and SN74AXC4T245- Q1?
Is there a reason a Pullup Resistors is needed to keep device disabled during power up.Is possible that OE can always be kept to GND?