Part Number: SN74AXC4T774 Other Parts Discussed in Thread: TXU0304 1.Part number: SN74AXC4T77
Only the transmission delay from port A to port B is indicated in the datasheet;
But can you provide skew parameter between channels A1-B1 and A2-B2?
Part Number: SN74AXC4T774 I considered replacing the 74AVC4T774 with SN74AXC4T774 (as TI recommends)
I read in the E2E the following thread
SN74AXC4T774-Q1: SN74AXC4T774QPWRQ1 - Logic forum - Logic - TI E2E support forums
Can you tell me how this investigation…
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: SN74AUC34 , SN74AUC2G34 Hi,
I want use a SN74AXC4T774PW to drive many SPI device.
How many device can be drive??
System spec.:
1: level shift 3.3V => 1.2V
2: use the many SPE_CS pin to select…
Hello Gordon,
Since we haven't heard from you if the simulation works or not, I will be closing this thread. If there are issues that come up in the future please let us know by opening a new thread. Thanks!
Regards,
Josh
Part Number: SN74AXC4T774 Hi :
I was using level Translator p/n SN74AXC4T774PWR for SPI application as SPI master and Slave are working at different IO voltage level.
I have downloaded the IBIS model from TI website and used ADS platform for IBIS simulation…
Part Number: SN74AXC4T774 Hello expert,
my customer has a request to have a redriver solution to enhance their NCSI signal. Below is the demonstration for the board layout and setting. Could SN74AXC4T774 used in this application to enhance NCSI signal…
Part Number: SN74AXC4T774-Q1 I have many questions about SN74AXC4T774-Q1. Please answer below.
Qestion.pdf
Above table is 6.13 Switching Characteristics, VCCA = 3.3 ± 0.3 V.
Q1:What's the reason the value varies 0.5 to 8 ? (For example tempurature…
Part Number: SN74AXC4T774 Other Parts Discussed in Thread: TXB0104 , , TXU0304 Hi team,
for SPI application,
seems like both TXB0104 and SN74AXC4T774 both can work
1. does this mean if we use SN74AXC4T774 on SPI , we need extra signal to control the direction…
Part Number: SN74AXC4T774 Hi Team
Can you explain why there is diiference between the UQFN and WQFN and only the WQFN has thermal pad?
Is there any frequency restrictions between components?
Regards,
Roey
Hi Ohashi,
Ryoma Ohashi said: When you look up to figure 9.2 in the datasheet, I can see that tpd for rise time and fall time differs respectively. So, tpd for rise time and fall time might differs in the real condition, right?
Questions:
The tpd for…