Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: SN74AXC8T245 We use SN74AXC8T245 to translate RGMII signals.
Port B link to PHY IC, VCCB is 1.8V.
Port A link to FPGA, the Bank voltage is 1.2V, so VCCA link to 1.2V.
Ethernet input is 1GHz…
Part Number: SN74AXC8T245-Q1 Hi Expert,
My customer is using SN74AXC8T245QPWRQ1 in their project. When they do the Propagation Delay timing test , VCCA=1.8V , VCCB=3.3V ,the delay between B6 → A6 ( UART_TX )is more than 4n.
In actual the sourcing and end …
Part Number: SN74AXC8T245-Q1 Hi,
I'm looking at the SN74AXC8T245-Q1 datasheet Table 8-1 functional table. I wanted to confirm that if this table is correct? I wanted to verify the accuracy of bits 5:8 direction base on DIR2. I've added a screenshot,…
Part Number: SN74AXC8T245-Q1 Other Parts Discussed in Thread: SN74AUC245 , SN74AXC8T245 Hi,
Good Day.
Customer would like to use SN74AXC8T245-Q1 in an RGMII application with 1.8V to 1.8V translation.
The data rate mentioned in the datasheet is "Up to…
Part Number: SN74AXC8T245-Q1 Hi, team
What's the maximum delay difference time between channels? Customer require <3ns, can we meet this requirement?
Which means give the inputs signal at same time and the time difference between output signals…
Part Number: SN74AXC8T245-Q1 Hi team,
my customer are testing CAXC8T245QWRGYRQ1, and I saw we still have samples in stock for PCAXC8T245QRGYRQ1,
what's the difference between those two? can they use PCAXC8T245QRGYRQ1 instead for test?